Part Number: DAC5578 Other Parts Discussed in Thread: DAC7578 , , DAC6578 Is there a software sequence that can identify whether the installed component is DAC5578 vs DAC6578 vs DAC7578?
Part Number: DAC5578 Hi team,
Please tell me about slave addresses.
Power is applied to AVDD, and the state of the ADDR pin is captured at the timing of POR release, at which point it is determined. After the slave address is fixed, there is no change…
Part Number: DAC5578 Other Parts Discussed in Thread: DAC7678EVM Hello,
Is there a sample project or software library for DAC5578? Can you forward it to me?
Thank you for your interest.
Good work.
Part Number: DAC5578 The data sheet for DAC5578SPW state "Capacitive load stability" is typ 1nF.
What would the implication if the outputs where loaded with 1uF in parallel with 680Ohm?
Is there a recommendation for serial output resistance if capacitive…
Part Number: DAC5578 Dear TI Team
There is the following description about Zero-code error. If you read this, is it correct to recognize that the Zero-code error changes depending on the output voltage?
Also, if the Zero-code error changes depending…
Part Number: DAC5578 Other Parts Discussed in Thread: DAC53204 HI Expert,
My customer is considering about the dynamic voltage scaling for DCDC output with DAC5578. (DAC5578 is reused from prior project)
https://www.ti.com/lit/an/sbaa342a/sbaa342a…
Part Number: DAC5578 Other Parts Discussed in Thread: DAC53401 Hi expert,
Customer is seeking for DAC with below sepc:
Channel number : >= 4 channel
Output type: current or voltage both OK, for both type, need DAC can sink or source current. For…
Part Number: DAC5578 Other Parts Discussed in Thread: DAC121C081 , , DAC43608 Hello,
I was guided to this forum by Jejomar Ildefonso from TI customer support. Here I found the following thread that might be related in some kind to our issue:
DAC121C081…
Part Number: DAC5578 Hi team,
This DAC5578 design spec maximun output voltage is 600mV. Please provide your review ccomment.
Questions 1. the EC send i2c_w rite 0x91 0x00 and oxffff 1 2, anything need to take care except this setting? 2. what is the…