Part Number: DAC5652AEVM Other Parts Discussed in Thread: DAC5652A Hi,
Is the HSDC Pro compatible with the Zynq-7020?
Planning to purchase the DAC5652A EVM. The data patterns will be generated using the Zynq-7020.
Please help!
Part Number: DAC5652AEVM Other Parts Discussed in Thread: DAC5652A Hi,
Was looking up how to interface and configure the DAC5652A EVM with the Zynq7020. Planning to generate the data patterns using the Zynq.
Anyone tried that here before? Any issues faced…
Hellow Hamza
There were the following questions from the Japanese customer who watched TI E2ETM Community.
Q1:The document"X2_Interleaved_Mode.pdf" is written as DAC5652, but is the inside circuit same in DAC5652A?
Q2:If there is official…
Part Number: DAC5652-EP Hello,
I'm looking for a dual channels DAC for a space radar. I need to use it at an update rate of 250MSPS. The ADC5652-EP is presented on the website with a maximum of 275MSPS, but the datasheet indicates it is "not production…
Sorry, reading https://www.ti.com/lit/ds/symlink/dac5652a.pdf again and Page 20 says for the 1:1 transformer, the expected output is indeed 500mVpp. So at least the board is working like it's supposed to besides the schematic / docs issue.
On Page 21…
Hi Mesh,
Yes there is no problem with the figure 22 in the datasheet.
Here is the link to the application note. Section 2.3 talks about how the compliance voltage for the DAC is calculated.
Regards,
Neeraj