Other Parts Discussed in Thread: DAC5681 , ADS5463EVM , DAC38J84 , 66AK2L06 , ADC12J4000 We are interested on the generation of a set of tones in I and Q components (i.e.: 10 tones, with possibility of tuning the frequencies separately) in the range 100-150MHz…
I would like to use TSW1400+DAC5681 to generate a sweep frequency signal, from the 150M-250M. scan time of 8 Microsecond, triggered by an external pulse signal.
I would like to confirm that an external pulse signal, triggering a sweep frequency, the…
Other Parts Discussed in Thread: DAC5681 Hi,
I'm designing a board with the DAC DAC5681. Reading the user guide in which there's the electrical drawing of the EVB, I need the balun transformer at the DAC output to have a single-ended 50 OHm net. This is…
i have an FMC110 card that we have been trying to get a DLL lock on for quite sometime. The Clocking is as follows: the AD5917 sends us a 200MHz clock on a pin configured for the card, and the DAC gets clocked at 400MHz, bit clock of the OSerdes is at…
Other Parts Discussed in Thread: DAC5681 Hello,
INL, DNL , offset drift and gain drift of the DAC5681 is specified at the condition of over operating free-air temperature range. Will these parameters be improved at the narrow temperature range(for example…
Other Parts Discussed in Thread: DAC5681 , DAC3484 , ADS5400 , DAC5681Z Hello,
The DAC5681 has an 8-deep FIFO in the datapath.
Register "OFFSET1" allows one to select the reset position of that FIFO pointer in bits 2:0 of that register. The description in…
Luis,
Take a look at the following app note. There is a section about using a 25 MHz reference. Perhaps you can just try the filter settings shown in there.
http://www.ti.com/litv/pdf/scaa113
Second, I'm wondering what would happen if you changed your…
Other Parts Discussed in Thread: DAC5681 Hi Hamza,
For DAC5681,should I use default values defined in data sheet from page 19-23 except for Config0 and Config10?
1) freq < 125MHz , Config0=1F, other wise 5F
2) Config 10 varies with frequency accordingly…