Part Number: DAC5682Z Dears.
I am reviewing DAC5682Z design.
Is it possible to set it to DAC5682Z? I want to input the IQ 250MSPS to the DAC5682Z and output the center frequency 312.5Mhz.
Can I do the following with the DAC5682Z Output?
Thank you.
Part Number: DAC5682Z Hi all
I connect DAC5682Z and FPGA through Parallel LVDS,Now I can output sinusoidal waveforms. When the Sin wave frequency was 4MHz, the Voltage value was 1.98V. When the Sin wave frequency was 250MHz, the Voltage value was only…
Part Number: DAC5682Z Hi
I am currently working on a university project and want to use the DAC5682Z.
I have a question regarding the voltage level of the digital data input D[15..0]P/N.
The signal is generated from an FPGA as an LVDS 1.8 V signal. Can…
Part Number: DAC5682Z The output of DAC5682z is full of glitches once the devices power on. The output is as shown in the figure below.
When I give the DAC a 2.5MHz sine wave, the output of dac can probe the sine wave, however, the glitches have always…
Part Number: DAC5682Z Other Parts Discussed in Thread: DAC5674 I am currently working on a University project, and would like to use the DAC5682Z.
I have read the datasheet and the user guide for the evaluation board, but there are Things i do not understand…
Part Number: DAC5681Z Other Parts Discussed in Thread: DAC5682Z , , DAC3152 Hi,
There are issues for TSW3100 and DAC5681Z.
TSW3100
At start, tftp is not excutable batch file in console window.
DAC5681z
could you provide example file to load in DAC5682z…
Part Number: DAC5682Z Other Parts Discussed in Thread: LMH6702 Hello, I am planning to use DAC5682 in our system. Output from device will be single ended +/- 0.5V signal. Client need to have DC coupled solution and I'm not sure to about output amplifier…
Part Number: DAC5682Z Other Parts Discussed in Thread: CDCE72010 , Hi,
We have DAC5682Z DAC on FMC interfaced to Virtex 6 FPGA and CDCE72010 for input clock. I have been using it at 250 MSps for generating waveforms without any problem for a few years.…
Part Number: DAC5682Z Hello TI-team,
I am considering using the DAC5682Z for an AWG design, which will use the DAC in different modes (with and without interpolation) and with a user configurable input data and clock rate. When using interpolation we…