Other Parts Discussed in Thread: DAC60004 , OPA4188 , LMH6321 Hello everyone,
For certain application, we need analogue output complying with following characteristics
Basic output from DAC60004
Software selection between:
Unipolar : 0 Vdc to 10 Vdc
Bipolar…
Hi Uttam,
Thanks for your timely reply. My customer's need is:
1. Dual channel is better.
2. 12 bit.
3. Bipolar output.
4. Voltage output.
5. Zero output during start up.
I can see DAC60004 is not bipolar output , which can not be accepted by our…
Part Number: DAC80004 Other Parts Discussed in Thread: DAC60004 , Team-
We have a customer who is applying 1.5V to VREF; in this case VDD = 3.3V
The data sheet states that VREF,min = 2.2V.
The question is what sort of derating should we expect in the converter…
Part Number: TIDA-01352 Other Parts Discussed in Thread: DAC60004 , LM5030 Hi,
Initially, our ultrasound system is planning to support only B-MODE, CWD and PWD mode. Thus we don’t have Elastography mode that requires High voltage +/-150V with huge current…
Part Number: DAC70004 Hi there,
I have a custom board design where the LDAC pin is permanently pulled down to ground. I had assumed that I could do a "software LDAC" by writing to individual channels using the command "Write to buffer n (IE D27 - D24…
Part Number: DAC70004 Hi there,
Do these devices have internal clamp diodes on the output? I do not expect output currents of more than 10mA from the DAC and so this may be sufficient if there are internal clamp diodes to prevent the output swinging…
Part Number: DAC80004 Hello,
I'm trying to evaluate the DAC80004EVM and connect it to RPI3 module to SPI0.
I use python to control the DAC80004 but w/o success.
I'm not using signals CLR~ nor LDAC~
My code below:
import spidev import time import…