Hi Hank,
Please consider the DAC60004 or the DAC60504. The main difference between the two is that the DAC60504 features an internal reference.
Thanks,
Paul
Part Number: ISO7741 Other Parts Discussed in Thread: DAC60504 , OPA551 , , ISO224 Hi, I'm using TI's DAC60504 to create a bipolar signal (ref. slaa869) and a Howland current pump.
This bipolar signal is fed to the Op Amp's input
Currently…
Hi Sebastian,
I believe you should consider the DAC60504 or the DAC60004. The DAC60504 has an internal reference, and can have an output range of 1.25V, 2.5V, or 5V with its internal reference. The DAC60004 does not have an internal reference, so if…
Hi Jerry,
That information is not available for the TLV5614. We will not be able to provide it. If you would like to contact me directly to discuss the potential volume of this socket, please reach out to me at frost@ti.com. Otherwise, please consider…
Hi Harson,
Thank you for your query. We don't have IBIS or TINA model for TLV5614 as this is a very old part. I would recommend DAC60504 in case you have not already suggested them. Is there a specific reason why they want to use TLV5614 as compared…
Thanks, Garrett.
Garrett Satterfield said: 5us settling time
Q0. Is settling time equal to Sample/update rate (MSPS)?
Garrett Satterfield said: DAC60504 - 12-bit, 4ch, 5us settling time, QFN
I think this will be perfect, except for the packaging.
Q1. Can…
Part Number: TLV5614 Other Parts Discussed in Thread: DAC60504 Hello team,
We are using TLV5614 DAC in one of our design, when I power on and power off the power supply repeatedly, and I found some TLV5614 have issues as below:
1. The VOUTA~D of TLV5614…
Part Number: DAC104S085 Other Parts Discussed in Thread: DAC60004 , DAC60504 , DAC70504 , DAC7716 Looking a replacement to LTC2634, a quad 12bit with FSO above 2.04V (preferred closed to 5V) ,similr to DAC104S085, but with DAISY CHAIN OPERATION!!!!
Part Number: DAC80501 I am using the DAC80501 with the internal reference and a 3.3V supply. My I2C communication works correctly but I am unable to update the DAC output. What is going wrong?
Part Number: DAC80508 I would like to implement communication with the DAC80508 on my microcontroller, do you have any examples that will help me get started?