Part Number: DAC60508 Hi!
I will use DAC60508.
I plan to connect a 1m lead from DAC60508 on the circuit board to the data logger.
The document of DAC60508 says 2kΩ and 10nF load to GND is possible,
so is this case OK?
Part Number: DAC60508 Dear Specialists,
My customer is considering DAC60508 and has a question.
I would be grateful if you could advise.
---
DAC60508 is used as the bias voltage of analog IC. See the circuit diagram below.
The DAC output voltage is set…
Part Number: DAC60508 Other Parts Discussed in Thread: DAC80504 , DAC81408 Hi there,
A few questions about the DAC60508:
- When writing to the LDAC bit in the trigger register, when exactly are the outputs updated with the contents of the buffer register…
Part Number: DAC60508 Hello,
Datasheet specify DC output impedance, 0.085ohms(typ) with midscale output and 15ohms(typ) with DAC output at GND or Vdd.
Vout drops as follows due to the DC output impedance?
Vout = Vout target * load /( DC output impedance…
Part Number: DAC60508 Hello,
My customer uses one DAC60508 and a host communicates only the DAC60508 via SPI.
So the SPI interface is not shared with other device.
And they do not use asynchronous update, only use synchronous mode.
In this case, can…
Part Number: DAC60508 Dear Specialists,
My customer is considering DAC60508 and has a question.
I would be grateful if you could advise.
---
I'd like to use an external REF(3.3V)
(1) When the device powers up, CONFIG Resister bit[8] is 0, this means…
Hi Lee,
This is not exactly the case.
Lee SungYun said: DAC80508 (16-bit) is 1/5 us = 200 kSPS, DAC70508 (14-bit) is 1/5 us * 4 = 800 kSPS, DAC60508 (12-bit) is 1/5 us * 8 = 1600 kSPS = 1.6 MSPS.
Settling time is a spec of the output buffer that consists of…
Part Number: DAC60508 I'd like to drive the DAC60508 outputs to the VCC rail of 3.3V+/-5%.
Can I connect VREF to VCC with DIV=2 and GAIN=2 without getting a reference alarm condition that shuts down the DAC outputs.
I see you have divided the Vrefin…
Part Number: DAC60508 Hi Uttam,
By the datasheet to get Gain = 2 (Max out voltage 2*Vref, need to set BUFF-GAIN = 1, REF-DIV = 0.
I did it, but the device output is 2.5V instead of expected 5V by this setting.
Why?