Part Number: DAC61404 Other Parts Discussed in Thread: DAC81404 , DAC81402 , DAC61402 Hi Experts,
Seeking your assistance on this query from Cx about DAC61404 device ID.
I'm currently working with the DAC61404 to create a threshold voltage for a comparator…
Part Number: DAC61404 I asked the question earlier if unequal voltages could be utilized when using the sense lines and was told it would be fine. We are seeing the devices latch up. When there is an offset on the sense lines I am seeing the device latch…
Part Number: DAC61404 I can read/write the SPICONFIG register (and read-back to confirm), but whenever I write to the DACPWDWN register it only ever reads back as 0xFFFF. According to the datasheet the lower 4 bits are R/W. Specifically, I am trying to…
Part Number: DAC61404 I would like to run the DAC in the 0-40V mode using up to 30V output. I also need to support compensation for the negative sense line to -2V with respect to the GNDs. Since the bipolar setup is only to +20Vout, I would like to run…
Hi Sarah, I see DAC61404 in your schematic and in E2E thread you have mentioned DAC61401. Which device are you using, DAC61401 or DAC61401? As you have DAC61404 in you schematic, i would Assuming you are referring to the same. Before i can help with debug…