Part Number: DAC63204EVM Tool/software: Hello
I am using a DAC63204EVM Dev kit. I can get a 10KHz sin wave using the included software but when I try to generate the sin wave using an external reference the board sems to lock up. I have removed the…
Part Number: DAC63204EVM Tool/software: Hello,
I use DAC63202RTER IC in my hardware design and my communication interface is SPI. I would like to ask you; Should I put the external pull-up resistors on the serial data output line and the chip select…
Part Number: DAC63204EVM Hi,
When starting communication and read the GENERAL_STATUS, i get 0x3E04. That's means all my 4 channels are busy and I can't send command like start/stop or managing signal amplitude. My device is unlock but impossible to…
Part Number: DAC63204EVM Tool/software: Hi,
My customer is using the SMART-DAC-EVM-GUI-Installer and downloaded the DAC63004WCSP-EVM-GUI and installed the control SW. However, they cannot communicate with the card.
They already downloaded SMART…
Part Number: DAC63204EVM Other Parts Discussed in Thread: DAC53202 , DAC63204 Hi,
I am trying to communicate stm32 nucleo board to DAC63204EVM over spi. Hardware setup is as follows:
1. SCK (STM32 nucleo board) to SCLK( DAC63204EVM)
2. MOSI (STM32…
Part Number: DAC63204EVM I have an issue with DAC63204EVM-GUI and SMART-DAC-EVM-GUI.
after installations, I got this message (for both GUIs): what should I do?
Ariel
Part Number: DAC63204EVM Tool/software: I am getting the same issue tried on 3 different machine. I also installed the NI runtime 2024.
Thanks,
Sophin Soeurn
Part Number: DAC63204EVM Other Parts Discussed in Thread: DAC63204 , , DAC80516 Tool/software: Hi,
I've identified the DAC63204 for an application that would require to control multiple voltage channels, a minimum of 16, and potentially up to a hundred…