Part Number: DAC63204EVM Tool/software: Hi, I am having an issue starting the software. I installed it as an admin, run it as an admin, and even added the NI labview runtime engine because it was missing from the package. unfortunately this is the page…
Part Number: DAC63204EVM Tool/software: Hi I am having trouble generating an output voltage from this DAC.
In a related post, this was mentioned
"When you are not in demo mode, you can select read all at the top of the low level page to get the register…
Part Number: DAC63204EVM Hi,
We need to install DAC63204EVM GUI for voltage margining. while I am trying to install, facing the below issue.
Please provide the link for installing.
Thanks
S Sathya shree
Part Number: DAC63204EVM Other Parts Discussed in Thread: DAC63204 Hi,
I am trying to configure DAC63204 in voltage out mode, using internal reference with gain 1.5, not able to see any voltage out on DMM. Can you please help with register configuration…
Part Number: DAC63204EVM Tool/software: Hi,
On the DAC63204EVM Data sheet it references getting negative current from the device. Does this require a negative voltage input to AGND? Or is there some type of configuration that can allow it by powering…
Part Number: DAC63204EVM I created a python class to control my DAC63204EVM board. It is open source and is on GitHub. I have tested I2C and SPI reads and writes and have GPIO control also added. I added simple checks to ensure that jumpers are properly…
Hello,
Please zoom in so I can actually see what a single write command looks like. I should be able to see every SCL pulse.
I can't tell just from the python code you are sharing how the I2C is actually being written out to the device.
Best,
Katlynne…
Part Number: DAC63204EVM Hello, I'm using the DAC63204EVM with your GUI. I'm trying to generate a PWM signal. I connected the FB pin to a voltage divider to create VFB=0.5VDD and define the output as a triangle wave .I've set MH and ML values.…
Part Number: DAC63204EVM Hi,
I Try to Current margining in DAC63204EVM With Below Configuration
Registers|DAC_0_MARGIN_HIGH FF00 Registers|DAC_0_MARGIN_LOW 0000 Registers|DAC_0_IOUT_MISC_CONFIG 1000 Registers|DAC_1_MARGIN_HIGH FF00 Registers|DAC_1_MARGIN_LOW…