Part Number: DAC7750 Hi team,
Could you tell me about the settling time of DAC7750?
1. Datasheet mentioned the settling time in condition that 16mA step, to 0.1% FSR. Could you tell me about this condition more detail?
2. The customer would like to know…
Part Number: DAC7750 Hi team.
My customer is seeing the same input but different output.
The system load is 200Ω.
Ch1 : 17.2V(86mA)
Ch2 : 1.27V(6.8mA)
They are the circuits at output that referenced the data sheet(p.39 fig,62).
I have some question…
Part Number: DAC7750 Hi team,
Could you tell me how much the time will it take to complete the reset after LATCH toggling when POR event triggered?
Minimum is 40us?
Regards,
Yoshi
Part Number: DAC7750 Hi team,
I got 2 question from the customer. Could you support this?
1. When the alarm detection is working, what is the status of the IOUT? Keep output value?
2. If DAC7750's die temperature goes higher than 142C, the Alarm will…
Part Number: DAC7750 Other Parts Discussed in Thread: DAC43401 , DAC53401 , DAC7573 Hi team,
May I have your help to propose a similar TI part with DS4422/4424? (2 and 4 channels)
It seems like we only have DAC7750/7760 are SPI interface, do we have I2C…
Part Number: DAC7750 hi sir
When the AVDD is 24 v input, the output current is 24mA
When the AVDD down to 12v, the output current down to 16mA
Does it's right?
how to maintain the output current whether AVDD(10~30V)?
Part Number: DAC7750 SnapEDA commented that the GND connections are differentiated on the datahseet, but given the same name.
GND and GND are labeled for both AGND and DGND.
There is a AVDD and DVDD to differentiate the Power supply connections, and this…
Part Number: DAC7750 Hello team From a customer, a question came. Of the following URL www.ti.com/.../sbas538c.pdf Three items of 8.3 Recommended Operating Conditions of DataSheet Page6 have following mention. Loop compliance voltage 4.95V(MIN) ~ 5.05V(MAX…
Part Number: DAC7750 Re: DAC7750
The Problem: We have a proto which is set up with
DVDD = 3.3V; DVDDEN tied to GND
AVDD=12V
REFIN tied to REFOUT
External ISET with R=15K
CONFIG = CALEN
CONTROL = ISET_EN + OUTEN + RANGE_0_20MA
GAIN_CAL = 0x8000
DATA …
Part Number: DAC7750 I will be implementing this part in a design without a HART interface. What do I do with the HART input pin? Float, connect to GND or 3.3V digital or 12V analog, or connect through a capacitor to GND? The data sheet SBAS538B of 12…