Part Number: DAC7760 Hello,
My customer has a question for CLR input signal of DAC7760. The below waveform is the CLR signal( CH3:Purple) and IOUT signal(CH1; Blue). CLR function itself works well from this waveform. They don’t have any problem as of now…
Part Number: DAC7760 Hello,
I want to implement a solution with 2 DAC7760 with only one output each one (0-24mA and 0-10V). I want it because it may be used at the same time with different output values.
My idea is to share the SPI bus with 2 CS, I think…
Part Number: DAC7760 Other Parts Discussed in Thread: ADS8681 , , DAC8760 Hello,
I took over a design, which was started by another engineer. Currently, the DAC7760 and ADS8681 are on the same SPI bus. However, as I am reading the DAC7760 datasheet, what…
Part Number: DAC7760 Hello,
My customer would like to know min value of hysteresis voltage that is defined in the datasheet like the below. Is the min value available?
Regards, Oba
Part Number: DAC7760 Hello, I have a question for DAC7760 specification. The datasheet says that DIN pin and SCLK pin are Schmitt-trigger inputs. Usually parameters like V_T+/V_T-/Hysteresis(V_T+ - V_T-) are specified for Schmitt-trigger inputs. But this…
Part Number: DAC7760 I have question about DAC7760 chip.
In user calibration,
1. In DAC7760, User calibrationc CODE_OUT is represented follows?
CODE_OUT = CODE*(User_GAIN + 2^11)/2^12 + User_ZERO
2. User_ZERO is represented signed value -> Then, the…
Part Number: DAC7760
Hi, I'm triying to use dac7760 and alarm pin is always in low state so dac not work. when i try to read status register there is no data come from dac. Is that mean dac was damaged or is there any other thing that alarm pin need…
Part Number: DAC7760 i'm trying to use dac7760 with STM32f1 and this is my schematic
I use the following function to send data from STM32f1 to a DAC7760:
static HAL_StatusTypeDef WriteSingle_DAC7760(uint8_t ch_Addr, uint16_t ch_Data){
uint8_t…
Part Number: DAC7760
Hi,
I would like to know what would be maximum number of devices in daisy chain configuration?
I currently have 6 without any problems but I have an application where 24 are required.