Part Number: DAC7811
Hi,
I am working on a system using the DAC7811 to generate an output from 0 to 2.5V. The system has already input voltages of +15V and -15V .As I have to generate a DC voltage just for the DAC VDD, I would like to know what is the…
Part Number: DAC7811 The DAC7811 datasheet refers to the ability to interrupt a command by de-asserting SYNC/ before the 16th falling edge of SCLK. Do I explicitly need to issue a "Daisy-Chain Disable" command before the SYNC Interrupt will work correctly…
Part Number: DAC7811 Other Parts Discussed in Thread: DAC8811 , DAC8822 , DAC8820 Hi, Experts:
May I have a question of the reference multiplying bandwidth for the multiplying DAC DAC7811.
As the digital codes goes smaller, the current going out from…
hello..
i measured the output at TP2 there iam getting the 1.66V .
i can verified all the voltage and power connections and all MOSI and CLK and CS connection are connected properly infact the MOSI and CS and CLK i am getting at the DAC7811 ic i will…
Part Number: DAC7811 Dear Team,
our customer is looking of a DAC and the parameter search showed the DAC7811 as possible candidate.
However, we are struggling with understanding how the part with 50MHz maximum SPI clock can support a 5MSPS that is shown…
Part Number: DAC7811 Good morning,
We are currently using your following component : DAC7811
Are there errata sheets published for this component ?
Best regards,
Christopher
Part Number: DAC7811 Other Parts Discussed in Thread: LF353 Hi,
i am using DAC7811 for my project. i have given Vref 3.3 v and sending a command 0x1xxx to alter the output voltage but i dont see any change in the out.
i am using current to voltage conversion…
Part Number: DAC7811 Hi,
i am using DAC7811 for one of my project. My design is to feed Vref pin with 8v p-p sine wave ( 5 khz) and then control the amplitude , using a current to voltage conversion. i am sending commands in SPI but still there is no…
Part Number: DAC7811 Other Parts Discussed in Thread: TINA-TI , , DAC8820 , DAC7822 Tool/software: TINA-TI or Spice Models Hello DAC support team,
I would like to know whether the PSpice model for DAC7811 is available or not.
I only found the DAC8820 PSpice…