Part Number: DAC80501 Other Parts Discussed in Thread: DAC80508 , To ask a follow up question: does TI have any plans to develop a Linux driver for this chip? A driver for the Zephyr project already has been written: github.com/.../dac_dacx0508.c.
Part Number: DAC80501 hello.
I'm designing a circuit using the DAC80501.
Please let me know if there is a way to improve the output voltage is not output normally.
As a phenomenon, the farther away from the set data 8000h, the more it deviates from…
Part Number: DAC80501
hi sir
according to data sheet.
OUTPUT under the condition of SINK 10mA, footroom > 0.3 V, cannot approach 0V,
But if there is no SINK 10mA, that is, if a gain buffer is added to the output, what is the minimum…
Part Number: DAC80501
Hello, Let me confirm about below.
* According to datasheet, user can use both internal REF and external REF. However, if user want to use external reference, user need to change register setting by REF_PWDWN. Then, I have following…
Part Number: DAC80501 Is there Linux driver for DAC80501? It's for the Motion controller and Customer would like to get this for OS development! Thanks.
Part Number: DAC80501 Hi all,
I am currently looking through the possible resources that I can use with DAC80501. As this device does not have any spice model, may I ask how can I make use of the IBIS file to do my simulation?
Is there any free software…
Part Number: DAC80501
Hi Team,
My customer would like to use DAC80501 in their design if long term drift is acceptable. In the datasheet the following is stated:
Do you have data at higher temperature (e.g. 40°C or 50°C) as well?
This drift…
Part Number: DAC80501 I am programming to use DAC80501. I am using SPI mode.
However, the output is not output normally. The output is ON / OFF at about 4.5kHz.
At first, 0000h is written with the "GAIN" command, and then 8000h is written as DAC data.…
Part Number: DAC80501 Hi Expert,
Good day.
Please confirm if this app note would still work if the DAC there will be powered with 3.3V instead of 5.0V.
https://www.ti.com/lit/an/slaa869/slaa869.pdf
Thank you.
Regards, Archie A.