Part Number: DAC80502EVM Hello,
I am trying to install the dac80502evm software. Open opening the application is receive a warning saying "Unable to locate the LabVIEW Run-Time Engine". I clicked the link and installed the runtime and rebooted my computer…
Part Number: DAC80502EVM Hi
Please can you provide the CE/EU Declaration of Conformity for DAC80502EVM ?
The product is CE marked but the CE/EU Declaration of Conformity is not available on the T.I website,
Thank you
Part Number: DAC80502EVM I'm getting some weird behavior regarding the supply voltage. If I supply 3.6v or more on VDD through J2 then when I send SPI commands to set the DAC voltage (for example setting it to 2.0v), then it will properly set the voltage…
Sure,
Have you installed the DAC80502EVM GUI software? A few initializations happen when the USB2ANY is plugged into your computer and you run the GUI.
The blinking is vague so it's hard to know what the problem is. The USB2ANy user's guide says it means…
Part Number: DAC80502EVM Hi Team,
The user guide says the software tool can be downloaded via DAC80502EVM's product folder but I cannot find it. Please advise where I can download the file?
Thanks a lot.
Vincent Chen
Hi Katlynne,
Thanks for your help.
And sorry for the late reply.
There is currently no way to limit the REF5050 supply until the DAC is powered on.
In addition, the circuit this time is based on the "DAC80502EVM".
When "JP4" is set to "short…
Part Number: DAC80502 I want to use DAC80502 for both SPI communication and I2C communication like DAC80502EVM. I plan to use 5V as VDD and 3.3V as digital logic power supply. Can I2C communication work when VDD is 5V and A0 pin is pulled up at 3.3V? …