Part Number: DAC80504EVM Hi Team,
Our customer is requesting for a sample code to control DAC80504EVM from TMDXIDK574 evaluation module. Do we have a sample code for DAC80504EVM?
Regards,
Danilo
Part Number: TMDSIDK574 Other Parts Discussed in Thread: USB2ANY Hi Team,
Our customer is requesting for the schematic diagram for the connection of DAC80504EVM to TMDSIDK574.
Regards,
Danilo
Part Number: DAC80504EVM Hi,
I am looking for the Altium design file of the DAC80504EVM. Need this to integrate with rest of my designs to design the product. Can you help me to obtain the files.
regards,
-ali
Part Number: DAC80504EVM Hello everyone,
I am working with DAC80504EVM. I want to establish the basic SPI communication between it and Arduino Uno. Currently, the DAC outputs give the midscale value after power up (GAIN = HIGH (2), REFDIV = HIGH(2), RSTSEL…
Part Number: DAC80504EVM Tool/software: Code Composer Studio Hello everyone,
I am working with DAC80504EVM and TMDSEVM6657. Currently I am trying to connect them via SPI (just a simple signal generation).
I am having problems with coding, as I am experiencing…
Part Number: DAC80504EVM Hello everyone,
I am using evaluation board DAC80504EVM in order to generate ultrasound signals which to drive three ultrasonic transducers. I would like to generate bipolar signals. However this DAC supports only unipolar signal…
Part Number: TMDSEVM6657
Hello,
I would like to interface DAC80504EVM and ADS8920BEVM with TMDSEVM6657 via SPI. My initial idea was to use SPI interface available on PH1 connector of the EVM. However, I see that CS1 is connected to FPGA and also to PH1…
Part Number: DAC80504EVM Hi Team,
My customer is looking for the possibility to log the data acquired with this board to Python/Matlab/Labview to process real-time, is this possible? Do we have a guide to this?
Thanks in advance.
Regards,
Renan
Part Number: DAC80504EVM Hello,
I would like to make a system which generates three different signals at the same time. Currently I am working with DAC80504EVM and as far as I have understood, with this DAC I can either have delayed transmission of three…
Part Number: DAC80508EVM DAC80508EVM do not work.
1) Power on reset.
I understand DAC80508M is used on DAC80508EVM, the DAC output (out0) initial voltage should be 1.25V, but it is near 0V at the power on.
I tried two cases of power-on as the follows…