Part Number: DAC81408 Dear, support Team. I have a question about the potential of the REFGND and GND pins of the DAC81408. Which is the reference potential of the analog output terminal, REF GND or GND? The background of my question is that the DUT connected…
Part Number: DAC81408 Other Parts Discussed in Thread: OPA2187 , Dear Technical Support Team,
There is Figure 67. Schematic for Remote Ground Tracking on datasheet page 46.
Do you have this accuracy between REFGND PIN and REF PIN?
1kΩ resistor are…
Part Number: DAC81408 Hi Experts,
We need your assistance with our customer.
(Please Note: For this case, VDD = VAA = +5v)
On the DAC81408, can Vcc = +5.8v and Vss = -5.8v for +/-5v and +/- 2.5v output operation or, does Vcc absolutely need to be…
Part Number: DAC81408 Hi,
I am considering using Streaming mode to update registers 14h to 1Bh.
Which is shorter, the data update wait time using LDAC or the data update wait time in Streaming mode?
When using LDAC, I recognize that TDACWAIT is…
Part Number: DAC81408 Hi,
I would like to set up registers by below methods, could you please answer my questions?
1.Are methods for "initial register setting" and "update DAC output" true?
2. In initial register setting, Which is wait time "1"…
Part Number: DAC81408 Hi,
10.3.1.2.1 of the data sheet states "In both update modes a minimum wait time of 1 µs is required between DAC output updates.".
Is 1 us a mistake of tDACWAIT = 2.4 us?
Best Regards,
Nishie
Part Number: DAC81408 Dear experts,
Our partner procure these from franchise source with DC:2105+.
Parts were in tape and reel and kept in temp controlled environment.
They observed on random pieces picked from the same reel:
a. contamination…