Part Number: DAC81408EVM Hi,
We would like to use the DAC81408 for developing the battery testing equipment and was using the EVM to do the verification.
However, we faced some short circuit issue. Just wondering if there is a power sequence between VDD…
Part Number: DAC81408EVM Hi
I was trying to execute DAC81408EVM.exe on my computer to test DAC81408, however, after I double clicked DAC81408EVM.exe, a window popped out and asked me to install the labview runtime engine.
I have installed LVRTE2015SP1_f13Patchstd…
Part Number: DAC81408EVM Hi,
Good Day. Is there a way that the customer can make their own custom GUI/ send a series of commands to the DAC81408EVM using the USB2ANY? Possibly in Python or Labview? Please advise. Thank you very much.
Best Regards,
Ray…
Part Number: DAC81408EVM
I have a question from a customer.
Hi, so I'm having trouble getting the DAC81408EVM to output anything when it's connected to an external master device (Protocol Analyzer on Analog Discovery 2). The DAC outputs correctly when…
Part Number: DAC81408EVM Hi Team, Our customer is currently experiencing an issue similar to the original thread. Below is the detailed information: "Currently using DAC81408EVM and a USB2ANY device. I have the hardware set up correctly, I'm assuming…
Part Number: DAC81408EVM Hi,
after connecting with USB2ANY, EVM application shows as DEVICE connected,
for read all command,
1.DeviceID: 298h
2.STATUS reads value 0x0008.
3.SPICONFIG reads value 0x0A04.
in DAC81408 page, changed DACOUT, but not able to…
Part Number: DAC81408EVM Hello,
I'm using the DAC81408 for common mode voltage and LO nulling on IQ modulator with differential IF inputs. Output pins of the DAC are resistively connected to the IQ modulator and the DAC adds 5 dB of noise when turned…
Part Number: DAC81408EVM Hello,
I got a bit confused with Vcc and Vss supply of the DAC81408. There is a note in the evaluation boar manual saying that 9 V < (Vcc-Vss) < 43 V.
But also there is an example in the datasheet showin Vcc = 21.5 V and…
Part Number: DAC81408EVM Hello,
I'm trying to control the DAV81408EVM with USB2ANY interface adapter and GUI from DAC81408EVM software downloaded for the TI website.
The connection is established, it seems that commands are sent and written (I can…