Part Number: DAC81408EVM I recently bought a DAC evaluation board, the DAC81408EVM, from TI. My problem with this board is that I can't get an output voltage, no matter what channel I choose. The communication with the DAC works fine, I attached a signal…
Part Number: DAC81408EVM Hello Guys,
Do we have mechanical drawings for DAC81408EVM?
We need the outer dimensions and the dimensions of the mounting holes and the spacing in between them.
Thanks!
Art
Part Number: DAC81408EVM I have problem writing to the configuration registers on DAC81408. I can read the registers but cannot write to it.
For example, when I send the command 0x83000000 through the SPI interface, I can read the (SPICONFIG register…
Part Number: DAC81408EVM Hi Guys,
I need 8 independent sinusoidal wave with the same frequency of 277 Hz and different amplitude varies from(-1:1) to (-10:10) volt. It means the amplitude of these 8 channel should be controlled and changed by MCU.
I…