Part Number: DAC8411 I have a DAC8411 DAC which only goes to from 0 to 1.65V. Upon sending 0b00100000,00000000,00000000 or any larger value, the DAC will go to zero volts.
I am not sure what is causing this problem, but need this device to go from 0…
Hi Paul,
Thanks for the quick response. I am using the DAC8411 Eval board. I have come to the conclusion that the DAC8411 on the board is damaged. I have the Jp2 connected to the 3.3V supply and with nothing connected to the SPI lines except 1K pull…
Part Number: DAC8411 Hello Team,
Our customer is considering using DAC8411 @ VDD = 4V with a 3.3V SPI.
What is the Serial clock frequency in this case, 20MHz or 50MHz?
I think it is 50MHz on the datasheet, is that correct?
Regards,
Masakazu
Part Number: DAC8411 Dear TI team,
I wan to confirm MSL level of DAC8411IDCKR, the part I received is MSL1, and date code is 1918+. But in your datasheet, it shows MSL 2.
So which MSL is correct? Loking forward to your reply.
Thanks!
Fred Che…
Part Number: PSPICE-FOR-TI Other Parts Discussed in Thread: DAC8411 , , TINA-TI Hi,
I was trying to build a 0-20mA current output DAC using the DAC8411 PSpice model. The DAC8411 model has a 16-bit parallel interface on the digital side. What is the…
Part Number: DAC8411 Other Parts Discussed in Thread: DAC80501 Hi, Our customer is considering using DAC8411 @ Vcc = 5V with a 3.3V MCU. But in DS SPEC it seems impossible. Is it really not possible without level shift? In general, 3.3V input should be…
Part Number: DAC8411 Hello support team,
I have some questions regarding DAC8411.
Our customer is carring out the noise testing with DAC8411, and a strange phenomenon has occurred.
Operating the DAC8411 with noise superposed on the AVDD / VREF line…
Part Number: DAC8411 Hello,
I would like to know the power-up time from "power on reset" of DAC8411.
Data sheet has only the power-up time "coming out of power-down mode" (typ.50 micro sec.).
If possible, I want to know max.value of that power-up…