Part Number: DAC8551 From reading the data sheet for the DAC8551, I should beable to enter a number from 0-65535 and the Vout should range from 0-5V (I have it connected to a 5V supply). When I write an integer (connected to the CLK and MOSI and D7 pins…
Part Number: DAC8551 Other Parts Discussed in Thread: DAC80501 , , Dear TI support team,
Comparing Figure 32 the curve zero voltage sink capability of the DAC8551 datasheet with DACs having a compareable output stage (see DAC80501 for example) , the valures…
Part Number: DAC8551 Other Parts Discussed in Thread: DAC161S055 , , DAC8811 , DAC8811EVM , OPA277
Team,
We are trying to understand the device parameters that gives or influence the frequency of the output signal. Goal is to find out what is the maximum…
Part Number: DAC8551 Other Parts Discussed in Thread: MSP430F449 , Hi,
Came across the SLAA297 (interfacing the DAC8551 to the MSP430F449) on google but the pdf link to ti.com is broken.
Do we still have this app note available?
Regards,
Jake
Part Number: DAC8551 Other Parts Discussed in Thread: DAC80004 , DAC7678 , DAC8571 Hi everyone,
i have a small question i need to use a 16-Bit DAC for a battery design and connect it to my LDO to control my output voltage. between 0 and 5 Volt.
After the…
Part Number: XTR111 Other Parts Discussed in Thread: DAC8551 Hello,
I want to use XTR111 for converting 0V-3V input voltage (Vvin) to 0mA-20mA current output.
We have below queries:
1. As datasheet mentioned specified output current is 0.1 to 25mA, so…
Other Parts Discussed in Thread: DAC8551 Hello, all
Now we have some inquiries regarding DAC8551 from our customer.
Please refer to the items below, and feedback us with your comment.
Q1. Output voltage settling time
When referring "ELECTRICAL CHARACTERISTICS…