Part Number: DAC8564 Tool/software: HI Sir
May I know How to control the DAC8564 correct?
After power on the DAC8564, When I Can send the command to DAC8564?
thanks
Part Number: DAC8564 Tool/software: I am having trouble with my DAC8564, which is generating heat of just under 100 degrees Celsius. I suspect that the cause is the 3rd pin. Currently, I have four DAC8564s on a PCB set on a raspberry pi 5, controlling…
Part Number: DAC8564 Other Parts Discussed in Thread: OPA333 , OPA317 , OPA391 , OPA191 , XTR111 , XTR300 HI SIR
I want to design a 4-20mA Function which use the DAC8564,
Did you have suggestion AMP for this?
thanks
Part Number: DAC8564 Hi,
Compilation environment: keil5 Using chip: DAC8564IDPW
1. Why is there a deviation in accuracy? Control channel A to output a voltage of 2V (DIN instruction is 0X10CCCC). The multimeter measured the voltage of Vout A to GND…
Part Number: DAC8564 Other Parts Discussed in Thread: DAC80504 Tool/software: Hello,
My customer is considering to use DAC8564, but the datasheet says IOVDD=1.8V(min) which means VIO=1.8V(typ) power supply can't meet the spec to think about the variation…
Part Number: DAC8564 Hello
I have (5) DAC8564 on one PCA design. I AVdd is 5V, and VioVdd is 3.3V. See image below.
I am having difficulty getting the DAC's to use an external 4.096V Vref. I have disconnected the 4.094V source, until I can prove the…
Part Number: LM5149 Other Parts Discussed in Thread: DAC8564 Tool/software: Good morning, I'm using the LM5149 on my design of a variable output buck converter with the following specs: VIN = 54V VOUT = 0.8V - 50V IOUT = 15A (or 30A with dual-phase) The…
Part Number: DAC8564 Hi,
I am designing a board using the DAC8564 controlled by a Raspberry Pi RP2040. Initially all four channels were working, I am sure the SPI commands being written are correct as a different design using the identical setup has…
Part Number: DAC8564 Other Parts Discussed in Thread: DAC60504 My customer is interested in comparing the output response of this part with the DAC60504. Can you share the freq response plots for both?