Part Number: DAC8718 The user guide for the evaluation board suggests that the chip can be damaged by an incorrect power up sequence.
My question is, do I need to control power down sequencing to avoid damaging the chip?
Part Number: ADS1278 Other Parts Discussed in Thread: DAC8718 , Im planning to used ADS1278, DAC8718. Both are 8 channel ADC and DAC respectively.
My requirement is to drive these to device in a synchronous way, such that all ADC input channels should start…
Part Number: DAC8718 Other Parts Discussed in Thread: OPA1664 , I am using DAC8718SRGZT for one of the industrial application for the analog outputs i have used OPA1664 in voltage follower configuration. Op-amp output is connected to E/P converters. Now…
Part Number: DAC8718 Other Parts Discussed in Thread: OPA1664
Hi,
I am Using DAC8718 (U11 in image below) for one of the projects. Output of dac is connected to Opamp "OPA1664" in voltage follower configuration followed by protection circuit.…
Part Number: DAC8718 Other Parts Discussed in Thread: DAC8734EVM hello ,ti
now, i want use dac8718 chip to finish DA function.
can you send me the sample code,so that i can use this chip faster and batter。
thank you very much。
my mail…
Part Number: DAC8718 HI, I'm testing DAC8718 .
I got a problem that DAC8718 outputs error after power-on, the error output is zero and the right ourput is -15V. then It always outputs +15V when I try to control it.
Before, due to the unusual sag in the…
Part Number: DAC8718 Other Parts Discussed in Thread: TS3A5017 , DAC81416 Hi,
Can I use single DAC8718 and use SP4T switch (similar to TS3A5017) at each analog output, so I can have 32 outputs from single DAC8718.
If possible please suggest an analog switch…
Part Number: DAC8718 Other Parts Discussed in Thread: DAC7718 , Team,
this is a continuation of the previous thread about DAC7718 heating up to 45 degrees C when the negative -5V voltage is applied to AVss (through a 1kOhm resistor).
We now use DAC8718…
Part Number: DAC8718 Hello,
I found that the voltage output will appear in the state of full range after the chip is powered on.The power supply voltage is ±15V, the reference voltage is 5V, and the software program writes 0V, but the output voltage is…