Ibrahim,
I think the EVM works with the setup I described in the previous post. I connected the MOD_OUT to MOD_IN and ran the device in the same way. With this connection, in full duplex I re-connected the scope and looked at the MOD_OUT, UARTIN, and…
Part Number: DAC8742HEVM Other Parts Discussed in Thread: DAC8742H Hi,
I have connected the HART module to the evaluation board In loop-powered. How to check whether the HART module is detected or not? Please let me know if any commands check the detection…
Part Number: DAC8742HEVM Hi Team,
My customer want to interface external HART Modem to DAC8742HEVM for testing and they have 24V line out from Modem.
Can you please guide how to connect and test external HART Modem to DAC8742HEVM for testing.
Thanks, Shinu…
Part Number: DAC8742HEVM Other Parts Discussed in Thread: USB2ANY Hello, dear friends.
I have some problem with connecting two DAC8742HEVM to each other.
I'm using two DAC8742HEVM with SPI & HART interface. I try to transmit data from DAC8742HEVM №1 to…
Part Number: DAC8742HEVM Hello,
someone using scripting feature in the DAC8742HEVM GUI? Which version of Python excactly should be installed for using the scripting? I tried Python 2.7.18 and the neweest 3.10. Both versions and in both cases it doesn't…
Part Number: DAC8742HEVM Other Parts Discussed in Thread: USB2ANY Hi Team,
We have received this inquiry from our customer,
I have a question about the DAC8742HEVM. I'm not getting a modulator output in Hart mode. I'm testing the transmit in Hart mode…
Part Number: DAC8742HEVM Other Parts Discussed in Thread: USB2ANY I use DAC8742HEVM with default settings (HART mode, power supply from USB2ANY, SPI mode selected in GUI). From the DAC8742HEVM GUI in high level configuration I generate write or from Low…
Part Number: DAC8742HEVM Other Parts Discussed in Thread: USB2ANY Hi,
I wanted to communicate to the DAC8742HEVM with another microcontroller through SPI interface, and at the same time wanted to still have it connected to the USB2ANY interface so i can…
Part Number: DAC8742HEVM Other Parts Discussed in Thread: DAC8742H , PROFIBUS Hello Team,
My customer noticed that in the datasheet for the DAC8742H it specifies a shunt 0.022uF cap to GND and a series 4700pF cap on the MOD_OUT line (page 29). However, in…
Brian,
I think you can couple in a sinusoid just using an RC circuit, but it does seem a bit primitive to do it that way instead of using some sort of summing amplifier. I would definitely check the 2200Hz signal to make sure that it isn't further attenuated…