Part Number: DAC8750 Hello guys,
One of my customers is evaluating DAC8750 to replace AD5420 with the device.
For the evaluation, they have the following question.
Could you please give me your reply?
Q. Should HART-IN terminal be connected to GND directly…
Part Number: DAC8750 Dear all,
I would like to ask about Daisy chain mode in DAC8750's datasheet.
Our customer is considering using multiple DAC8750s in a Daisy chain connection (cascade connection).
They believe that when using a Daisy chain connection…
Part Number: DAC8750 Dear all,
I would like to ask about Rload in the following figure.
I have been asked by our customers how much Rload is acceptable.
The data sheet does not specifically describe the range of Rload, and only Rload = 300Ω is shown…
Part Number: DAC8750 Hi team,
I have got an inquiry from my customer, in as below.
- Could you please provide the histogram /w standard deviation value for some specs; at least, offset error, full scale error, and its temperature coefficient.
- Does the…
Part Number: DAC8750 Make a 4-20mA circuit in accordance with the circuit diagram in the manual. The unused pins are floating. It is advisable to ask if the EN1 EN2 of ISO7631 is floating or connec ted to the power supply.
Part Number: DAC8750 Other Parts Discussed in Thread: DAC8760 We are evaluating the feasibility of switching from the Analog Devices' AD5420 to the TI DAC8750. Initial results have been promising: we soldered an DAC8750 onto our board and had the…
I have not made that transition to the DAC8760 yet. I am waiting on samples. I have swapped out the DAC8750 and it was a drop in replacement for the AD5420. I ran it with an external rset and without. I did alter my startup code so I would not activate…
Part Number: DAC8750 I have my first run of product using the DAC8750. While all prototypes function correct, I have a few where SPI data does not go through. In my code I continually update the control, config and DAC registers about once every 1.6mS…