Part Number: DAC8750 Hi team,
We are struggling to understand why there is a difference between the measured current output and the assumed current output.
We assume that the current output accuracy is within +/-0.18%FSR. How to get the number is below…
Part Number: DAC8750 Hi team,
We would like to understand the definition of TUE in DAC8750 datasheet.
1. Does TUE specification include INL, Offset Error and Gain Error? We are confused this because the datasheet has TUE and also INL, Offset Error and…
Part Number: DAC8750 Other Parts Discussed in Thread: TIPD153 , DAC8760EMC-EVM In the DAC8750 data sheet on page 36 figure 62 they show an application for factory automation with protection on the output of this 4-20mA DAC. Two back to back schottky diodes…
The software is now working. We are having problems with some DAC8750's that quit outputting current; the current is reduced to 0.05 milliamps. 5 or 6 DAC8750 have been replaced.
The circuit is the same as the eval board, but with CAP1 = 0.47uf and…
Part Number: DAC8750 The datasheet says:
Resistor RSET (used to convert the DAC voltage to current) shown in Figure 53 determines the stability of the output current over temperature. If desired, an external, low-drift, precision 15-kΩ resistor can be…
Part Number: DAC8750
Hello,
we have a problem with the Daisy Chain mode of the DAC8750. We have 4 DAC's in daisy chain mode and it works well but after some days or weeks the output of the 3 dasy-chain DAC's are hold on the last value. The first…
Part Number: DAC8750 Other Parts Discussed in Thread: DAC8760 Hi,
I would like to to use the DACx760EMC-EVM to generate analog output controlled by a PC. I wonder what is the maximum output frequency that I can get from the DAC8750 using this setup.
Thanks…
Part Number: DAC8750 Hello.
The datasheet says:
8.6.1.4 Reset Register The DACx750 reset register is written to at address 0x56. Table 17 provides the description.
Table 17. Reset Register DATA BIT(S): DB0 NAME: RESET DEFAULT: 0 DESCRIPTION: Software reset…
Other Parts Discussed in Thread: UCC15241-Q1 , DAC8750 Hi,
We have a requirement on Integrated Isolated DC-DC converter for the below specification. Kindly suggest the suitable part which meets the requirement.
VIN-24V
VOUT-24V
IOUT-200mA
Regards,
Chitharanjan…
Part Number: DAC8750 Hello,
We have 2 questions about DAC8750.
1.Daisy-Chain Mode
How many DACs can be connected? We'd like to connect up to 8 DACs.
2.CLR terminal
If unused, should it connect to GND or left unconnected?
Best Regards, itabi