Part Number: DAC8760
Hello All,
I'm working with DAC8760 in newly designed Hardware board. I'm trying to reset the chip by writing 0x560001 and configuring control register to 10v range
0x553001. I was using same steps as AD5422 chip's register…
Part Number: DAC8760 I'm having an issue where the part DAC8760IPWPR at 0 DAC counts is outputting 10mV when it should be outputting 0V. Does anyone know why this is and how to correct it?
Part Number: DAC8760 Other Parts Discussed in Thread: DAC7760 Hi team,
Do we have new device to replace DAC8760?
It would be better if it's a pin to pin solution.
Hi Ankush, To check what you mentioned, you are not getting the correct HART signal on the DAC8760 IOUT pin? Did you enable the REXT bit in the DAC8760 Control Register, since you are using ISET-R? (Field 13 of Reg 0x55) Thanks, Lucas
Part Number: DAC8760 Hello guys,
One of my customers is considering using DAC8760IRHAT for their next products.
At this moment, they have the following question about the device sample rate (update rate (sps)).
Could you please give me your reply?
Q. Could…
Part Number: DAC8760 Other Parts Discussed in Thread: DAC8775 , DAC8775EVM hi Sir
I need to design a AO module which need 2 ch output or 4 Ch output ver.
i see the ADI/AD5423, TI /DAC8760 meet my needs
AD5423 have the daisy chain, and DAC8760 remove the…
Part Number: DAC8760 Other Parts Discussed in Thread: OPA4170 , While using the OPA4170, we have to use the DAC8760. While doing so, what is the significance of the VSENSE pin both + and -?
Also, Why is a 5k ohm resistor used between VOUT and +VSENSE is…
Part Number: DAC8760 Other Parts Discussed in Thread: DAC7760 Hello guys,
One of my customers uses DAC8760 for their current products with daisy-chain.
Recently they received PCN of DAC8760 and they knew that "Daisy-Chain Operation" section and Daisy…
Part Number: DAC8760 Hi,
We have used DAC8760 converter earlier with unipolar supply (24VDC) and it has worked well.
Now we utilize this very same circuit for another application having ±12VDC supply. Below is schematics of the design. Currently…