Part Number: DAC8760
Hi Team,
We would like to use DAC8760 for “1V to 5V” and “4mA to 20mA” at OVR=1b.
--------
[Q1]
We would like to set “full scale voltage=around 5V” at OVR=1b, VREF=5V, GAIN=1, N=16.
Then, I have to set CODE of case3…
Other Parts Discussed in Thread: DAC8760 Hi Team,
We are debugging the functions of DAC8760 and it is normal. Now because of the requirements of anti-jamming, we hope to add CRC check to SPI communication.
We used the following CRC8 algorithm, and…
Part Number: DAC8760 Hi, expert
My customer is using DAC8760 pin to pin replace AD5421, but they found no data from DAC output.
They can write into the register to adjust the output current, but when they read the DAC data, the SDO is always low.…
Part Number: DAC8760 Hi,
If either 4-20mA or 0-5V output is used exclusively as the output specification,
is it OK if the AVDD voltage of pin 24 does not satisfy 10V?
If it is OK, how many volts can it drop?
Best Regards,
Part Number: DAC8760 We are writing through spi via arduino to DAC Input pins but not able to write anything on that and Output pins are also showing 24V continusly
Design File is attached.
[07] - Digital Output.zip
Part Number: DAC8760 Hi,
Could you please let me know the resister setting to realize below mode?
- Dual output mode : Enable DB8 bit in Configuration register. - Vout mode : Disable DB8 bit in Configuration register - Iout mode : ??
Are the setting…
Part Number: DAC8760 Other Parts Discussed in Thread: DAC8771 , LM7705 Dear Sirs,
Another problem/doubt about DAC8760...
I have to implement a 0-20mA solution and I have setted on 0-24mA option to obtain a useful range over 20mA full-scale.
What…
Part Number: DAC8760 Hi Team,
We would like to use user calibration for 1V to 5V.
We input signed 16-bit code(positive number) to User_ZERO.
Then, we can calibrate 1V side but 5V side clip (mora than 0xFFFF).
Therefore, we can't set it properly…
Part Number: TMUX7219 Other Parts Discussed in Thread: DAC8760 , Hi guys.
I am looking for a solution for protecting the voltage and current output of the DAC8760.
You can see the thread about DAC8760 trouble here .
The problem is that the customer…
Part Number: DAC8760 Other Parts Discussed in Thread: XTR111 , DAC8775
Dear all,
I'm wondering if there is a practical and safe solution to multiplex the DAC8760 analog output on three different outputs.
Basically I'm designing a 3-axis tilt sensor…