Part Number: DAC8771 Hello TI Team,
I am using the DAC8771 in voltage output mode. SPI communication appears to be working because I can enable the internal reference successfully. However, the buck-boost converter is not enabling and the output remains…
Part Number: DAC8771 Tool/software: Hi everyone,
we're currently working with a custom PCB that uses the DAC8771, and while basic communication and functionality seem to work, we're encountering a major issue: The output amplitude is far too low. After…
Part Number: DAC8771 Hi,
The DAC8771 does not have an enable pin.
I tried to limit power consumption of the DAC8771 in a basic application cirquit as shown in the datasheet paragraph 9.2.
By resetting the 0x02 and 0x07 registers ( set to 00000001…
Part Number: DAC8771 Tool/software:
I am currently facing two related problems with the Digital-to-Analog Converter (DAC) implementation:
No DAC Output Voltage via SPI Protocol: Despite sending commands via the SPI protocol, I am not observing…
Part Number: DAC8771 Hi,
My customer raised a complaint about a sudden surge of current consumption on DAC8771 when they trigger open circuit condition.
There are a total of 4x DAC8771. All 4 DAC are using same settings.
They connect the ammeter…
Part Number: DAC8771 Other Parts Discussed in Thread: OPA192 , , TLV9362 , OPA2990 , DAC8775 , Tool/software: Hi,
I’m working with the DAC8771 and would like to use its internally generated negative supply (via the integrated charge pump) to power external…
Part Number: DAC8771 Other Parts Discussed in Thread: DAC8760 Hello team,
Can DAC8771 output both voltage and current at the same time?
I see DAC8760 is capable of doing so. Below is from DAC8760 datasheet.
Best Regards, Kei Kuwahara
Part Number: DAC8771EVM Other Parts Discussed in Thread: DAC8771 , DAC8760 , DAC63202 Hi,
Is it possible to use the DAC8771EVM as a 1KHz arbitrary waveform generator? The datasheet does not specify maximum sample rate. Thus, I presume it is only meant…
Part Number: DAC8771 The data sheet for the DAC8771 on page 37 is given by equation 7 and the comment below it states:
"WHERE: GAIN is automatically selected for a desired voltage output range as shown in"
But I cannot find the reference in the…