Part Number: DAC8775 Hi team,
On equation 8, can you please help give an numerical example on how to calculate the slew time? For example -
Output change = -10V to +10V, i.e. 20V.
Step Size = 8 LSB (SR_STEP[2:0] = 011).
Update Clock Frequency = 200,000Hz…
Part Number: DAC8775 There are two questions about DAC8775 initial Programming.
1. Pls help to check if below setup is correct?
DAC8775_WriteToRegister(0x01, 0x0001); // Reset Register
DAC8775_WriteToRegister(0x02, 0x0012); // Internal Reference 5V…
Part Number: DAC8775 Other Parts Discussed in Thread: , DAC8565 , DAC8760 Hi team,
Hope you have a good hoilday!
My customer compared DAC8775EVM and their own design, and have below test result:
They set the full range at ±10V, and EVM only shows ±0.003V…
Part Number: DAC8775
Is it possible to operate DAC8775 with10V supply?
Require stability data of internal reference. Can you help to share or point in datasheet if part of datasheet?
Part Number: DAC8775 Hi,
According to the following E2E, DAC8775 requires 200us from asserting RESET to starting SPI access.
https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/843867/dac8775-how-long-does-it-take…
Part Number: DAC8775 Dear TI Team,
I want to know about the output update rate for four channels in parellel for DAC 8775. It seems it works fine till 1 kHz after that it is not worked properly and I saw some cliiping in signals.
Part Number: DAC8775 Hi gents
I am facing with an output of DAC8775 card, getting 0.0mA on any channel.
DAC8775 Schematic
DAC775_Schematics.pdf
Clock Configuration
Main.c (for getting 20mA out in Channel A)
Settings:
1. Clock Polarity(CPOL): High
…
Part Number: DAC8775 Dear community
For DAC8775, an API, driver or library to control it? Not to configure. An API to manage and control it (source code).
Best regards,
Benjamin Colomer
Part Number: DAC8775 Hi,
Could you please let us know the VOUT_x, IOUT_x pin status on the following conditions?
CASE1:
DVDD : Power_OFF
AVDD : Powered
VPOS_IN_x : Powered
VNEV_IN_x : Powered
CASE2:
DVDD : Powered
AVDD : Powered
VPOS_IN_x : Powe…