Part Number: DAC8802 Other Parts Discussed in Thread: DAC8820 , TINA-TI Tool/software: Looking for at least a basic model that includes power consumption and input output impedances, etc. for simulation.
Part Number: DAC8802 Hello team,
My customer requested the additional specification which is not stated in datasheet.
Can you provide below information?
10% to 90% settling time (input, output)
digital delay (= interface delay)
Spurious free…
Part Number: DAC8802 Dear DAC support team,
We have been using DAC8802 for probing internal controller parameters (FPGA-based controller). After generating the correct clock and CS pulses for the SPI protocol, the rest of the pins: MSB and RS\bar, were…
Part Number: DAC8802 Hi all,
I'm using the DAC 8802 SPI DAC on a project with a Xilinx Zynq SoC and Yocto.
I can't find an existing IIO driver in the latest release of the Linux Kernel:
https://elixir.bootlin.com/linux/v6.2-rc7/source/drivers/iio…
Part Number: DAC8802
Dear DAC support team,
We have been using DAC8802 for probing internal controller parameters (FPGA-based controller). After generating the correct clock and CS pulses for the SPI protocol, the rest of the pins: MSB and RS\bar…
Part Number: DAC8802 Other Parts Discussed in Thread: DAC8806 , OPA552 , THS4011 In the DAC8806 .pdf data sheet on page 13, There is a timing diagram. On the second line from the bottom, there appears to be an alternate timing diagram. Is that correct…
Part Number: DAC8802 Hi,
The maximum value of DAC8802 supply current is 5 microampere but the full-scale analog output current for 3FFFh is 2.5 milliampere.
Q1. Is it possible to operate DAC8802 from a voltage rail of 5V having 5microampere capacity…
Part Number: DAC8812 Other Parts Discussed in Thread: DAC8802 Hi Everyone
I'm working on a test solution for the DAC8812 and DAC8802 and I want to test continuity in the analog pins, however I want to make sure I'm doing the right thing. Referring…
Other Parts Discussed in Thread: DAC7552 , DAC8562 , DAC7562 , DAC8812 , DAC7716 , DAC8802 , DAC8734 Looking for dual 12/14bit loke DAC7552, but for +/-10V.