Part Number: DAC902 Hi,
I have an application requirement as follows:
The input signal fed to the DAC is LVCMOS CLK and 12-bit DATA.
The desired output frequency of the analog signal from the DAC is a sine wave with a maximum frequency of 45MHz…
Part Number: DAC902 Tool/software: Hi TIer
My customer have a ultrasound application which use AD9706 in TGC module.
They need some low cost chip in this project .
I search in TI.com and found AD9706.
However, I see DAC902 is old.
Do you have…
Part Number: DAC902 Other Parts Discussed in Thread: DAC2902 Hello,
What is its minimum sample rate? If I understand correctly its minimum sample rate is 125MSPS and we need minimum sample rate 80MSPS.
His evaluation board is DAC902EVM ? And it…
Part Number: DAC902 Other Parts Discussed in Thread: DAC5672A , DAC904 , DAC2932 , DAC7821 Hi expert,
Could you please recommend TI device to replace AD9744 and AD5445? Thanks!
Regards,
Jared
Part Number: DAC902 Other Parts Discussed in Thread: THS3091 , THS5661A Hello,
I want to generate a 500KHz sine wave using a DAC attached to microcontrollers GPIO pins (8-12 bits). I need these waves with smooth curve so i was planning to define around…
Part Number: DAC902 Hi all,
I've a couple of project that will use DAC902.
I'm wondering if it is possible to have the digital power supply at 3V3, while maintening the analog at 5V, in order to connect the digital parts of the DAC to an external…
Other Parts Discussed in Thread: DAC902 , DAC902EVM , THS5661EVM Dear Specialists
MY customer is considering DAC902 for RF transceiver.
He wants to know SFDR with a window at wider range.
Datasheet spec says only 2MHz or 4MHz span.
Could you please…