Thanks,
So just to be clear, If I want to run small programs/ algorithms, they can be designed for the DSP in the 1642, or using the Hardware accelerator in the 1443. However, for more complex and heavy computation it is recommend to use DCA1000 to…
Part Number: IWR6843 Other Parts Discussed in Thread: UNIFLASH , When trying to flash the IWR6843BOOST board using Uniflash 4.3.0.1802 on Mac OS Mojave 10.14 I find that it hangs before programming.
The software is able to 'discover' the correct board…
Part Number: AWR1843BOOST
Tool/software: Code Composer Studio
How can I read the binary file in matlab (compatible with DCA-1000 EVM), because there is no code provided specifically for AWR-1843BOOST (having an additional transmitter too). So if there…
Part Number: MMWAVE-STUDIO Other Parts Discussed in Thread: IWR1443 Tool/software: Code Composer Studio Hi,
I want to use IWR1443 and DCA1000 to detect the data immediately like the radar on the car.
How do I set up?
And if I want to use CCS to…
Hi Raghu,
1.Based on AWR1642boosr,I refered to MMWAVE-SENSING-ESTIMATOR ( https://dev.ti.com/gallery/view/1792614/mmWaveSensingEstimator/ver/1.3.0/ ).
Enter the parameters on the left side of the interface, and get the configuration parameters on…
Part Number: AWR1642BOOST Hi,
I am doing some experiments and find something interesting. Hope you can help me explain it.
1) I calculated the energy of received signal by summing the square of ADC samples' amplitude. I found that the energy is almost…
Part Number: IWR1443 Hi There.
A2D's number of bits was mentioned 12 bits in datasheet of IWR1443. However it has been also mentioned in this forum that output of DFE can be 12/14/16 bits.
I was wondering what is ENOB of the A2D and DFE combined?…
Part Number: AWR1843BOOST Other Parts Discussed in Thread: AWR1843 I am using AWR1843 + DCA1000 and while configuring board using mmwave studio i get below errors
[20:34:55] ***Script completed successfully.***
[20:50:57]
[20:50:57] &&&&&&&&&&&&&&&&&&&&…
Part Number: IWR1443BOOST Other Parts Discussed in Thread: INA826EVM
I have an IWR1443BOOST board connected to a DCA100EVM using the 60-Pin adapter. I have modified the DataCaptureDemo_xWR.lua file to continously transmit and receive data. I ran the…
Part Number: AWR1642 Hello again,
My understanding is that the devolopment kit comes along with SDK, instruction sets, and library (?) , and etc.
If we buy chips and develop our own board, can we still program the chips via TI provided tools? or is…