Part Number: AWR1642 Hello again,
My understanding is that the devolopment kit comes along with SDK, instruction sets, and library (?) , and etc.
If we buy chips and develop our own board, can we still program the chips via TI provided tools? or is…
Part Number: IWR1642BOOST In the serial data, we see some terms like this:
RangeProf[0]: 091.787 RangeProf[1]: 099.316 RangeProf[2]: 097.093 RangeProf[3]: 091.389 RangeProf[4]: 086.496
What do they mean?
I asked a question and got the following…
Part Number: AWR1642BOOST Tool/software: Code Composer Studio Hello,
Now, I am studying the data output of adcbuff through can interface, but I don't know the corresponding relationship between data format and receiving antenna in adcbuff,I hope you…
Part Number: AWR1243BOOST Other Parts Discussed in Thread: AWR1243 , MMWAVE-DFP Hello,
According to the AWR1xx_Radar_Interface_Control.pdf (mmwave_dfp_01_00_00_01) I try to calculate CRC of ENVELOPE to use AWR1243BOOST with external SPI controller.…
Part Number: IWR1443BOOST Hi,
I have the DCA 1000 and an IWR1443BOOST EVM. I would like to know if there is a way I can stream data from the DCA board to a linux system without using the GUI that TI has provided?
Thanks
Part Number: AWR1243 How do I set the AWR1243 into continuous sweep mode from within MM-Wave Studio? Do I need to set the number of frames to zero? I am trying to measure the radiated BW.
Gabriel
Part Number: AWR1642BOOST Other Parts Discussed in Thread: AWR1443 , AWR1642 , IWR1443 Hi,
Previously I was using IWR1443 with DCA1000 to generate micro-Doppler spectrograms. The results were so good. In order to measure human gait motion in 3D (x,y…
Part Number: IWR1642BOOST Tool/software: Code Composer Studio Dear All,
I recently purchased mmWave IWR1642boot when tried to build people counting demo using CCS v8 i am facing issue (attached below), while building dss two pre-build errors will appear…
Part Number: AWR1642 Tool/software: TI-RTOS Hello, I have followed the steps you said, but there is still a problem, the mss.main project can run normally, but the dss.main project can not run normally, the result is as shown below. Maybe I missed a certain…
Part Number: IWR1443BOOST Other Parts Discussed in Thread: IWR1642BOOST Hi,
I want to know what is the maximum number of points that a IWR1443BOOST and IWR1642BOOST can return?
Thanks.