Part Number: DCR011205 Other Parts Discussed in Thread: DCR010505 , TL7660 Hi,
I hjave use TL7660 as 5V to -5V converter in my old design. But there was a range ripple at -5V output, so i decided to change converter as DCR011205 (my system supply 12V also…
Part Number: DCR011205 Other Parts Discussed in Thread: DCR011203 I am using several DCR01 regulators in one of my designs. There are two sets of 3, one DCR011203 and two DCR011205s. Both sets have completely independent loads. They have sync pins tied…
Part Number: DCR011205 I am trying to generate an output 5V on DCR011205 for an ISO1050DUBR transceiver but it not present. On pin Vrec I see 7V and on pin (14) output a voltage of 0.6V approx. I supply 12V on both pins VS. Worth noting my GND and GND_ref…
Part Number: DCR011205 Hi everyone,
I am trying to use a DCR011205U to create 5V power rail but I can't achieve it. the chip doesn't output any voltage. I have tried to change it, the same issue.
Please find below my schematic :
Is there anything…
Part Number: DCR011205 Other Parts Discussed in Thread: DCR021205 Hello.
I'm designing a circuit and I want to add TWO DCR011205. I want to know if is it possible to connect both outputs (VOUT+) to have all the output current available in one single line…
Dear Tom!
When I started designing my circuit for DCR011205 I came across your post above, and used your schematic for noise reduction. However now after I have soldered everything together, I have measured with an oscilloscope (PicoScope 2205) the output…