Part Number: DCR021205 Other Parts Discussed in Thread: LM5180 Hi Team,
A customer is using DCR021205P however, the stock is very limited.
Now the customer is asking for an alternative solution for their design and would like to know if we can suggest…
Part Number: DCR021205 Other Parts Discussed in Thread: REG103 Dear,
We are promoting this part now, and we have several questions about it, so could you kindly help us check them?
This part has no OCP function, and only has OTP and short protection, so…
Part Number: DCR021205 Can you provide some info on TI PN DCR021205P-U, which is a 2W, 12V to 5V converter.
Occasionally, we get some parts that initially test ok with 5V output but when integrated in the next level assembly, the 5V fails, no output…
Other Parts Discussed in Thread: DCR021205 Hello,
I am using the DCR021205 isolated switching regulator for a custom PCB and am receiving some weird results. Currently, I cannot get the 5V rail to come online when the input voltage is around 12V. Dropping…
Other Parts Discussed in Thread: DCR021205 Sorry this is in the wrong forum but I could not find a Isolated DC/DC section.
I require an isolated power system to power a microcontroller, 4 Optocouplers, and some various sensors, approximately 3W.
…
Pablo:
DCR011205 is not compatible with current sharing. . Its regulated 5 Vout does not current share.
However, a single DCR021205 , 2w watt isolated converter with up to 400mA load regulated 5Vout is recommend for your application.
Tom
The schematic as drawn has -12V shorted to -5.2V. ThePTN04050C is not designed to have(-Vin to -Vout ).
The PT79SR152 is the only negative module non-isolated regulator available. It is still recommended for new designs.
The PTN04050C is not an isoalted…
Hi!
Thanks for the quick answer!
My scope has a 25MHz bandwidth and 200Msample/sec Sampling frequency. I have removed the ground lead, and the clip from the scope probe, and magic has happened, the noise is now around 10mV measured 10 cm away from…