Part Number: DDC1128EVM Tool/software: Dear TI,
Is there any update for the software of the DDC1128 EVAL board?
The revision running is: v3.0.4731.32745.
Thanks.
Part Number: DDC1128EVM
Hi guys,
Our company is evaluating the use of the DDC1128EVM. We would like to get the datasheet in PDF format to evaluate the technical features and understand if it is suitable for our needs.
Is it possible to have the…
Part Number: DDC1128EVM Hello Guys,
Good day.
Our customer is looking for the dimension and technical information for this evaluation board.
He is building a test system that has 100 channels per board, and there are about 150 boards total. If possible…
Part Number: DDC1128EVM Other Parts Discussed in Thread: DDC112 Hello
I would like to use the dual-channel DDC112EVM to measure two photodiode current signals.
With the photodiodes I measure the absorption of gas in the MIR region of light, where…
Part Number: DDC1128EVM Dear TI technical support, we would like to purchase the optimal wall power supply adapter for the EVM board.
J18 only accepts dc voltage from 7V to 10V. Is there any restriction on the output current or power rating of the ac…
Part Number: DDC1128EVM ear TI,
I developed a "Daughter" Interface board for DDC1128EVM for receiving very low DC signal signal from PCBs photodiode sensors.
I use coaxial cable with SMB connectors to receive the signals of the photodiodes from a…
Hi Praveen,
I can't get the EVM board to work at the highest sample rate. When analyzing the data, the actual sample frequency seems the set frequency/2. Could you please tell me how to configure the EVM software to use a sample rate of 6.25kHz. Please…
Part Number: DDC1128EVM Dear Experts,
I'm runing the software provided after NDA with Windows 10 64-bit machine. The software has been installed and works apparently well. The program starts and displays windows correctly. After system refresh of the…
I am trying to fetch data from DDC1128EVM using python script.
I am doing to without trying to configure the registers from DDC chip and FPGA!
Because of this my buffer is filled partially and not sure why.
Just want to know whether there is some…
Hi Matt,
Thank you for your reply.
I confirmed your email.
I could understand the meaning of the output data.
I appreciate your great help and cooperation.
Best regards,
Shinichi