Part Number: DDC2256A Dear e2e Community,
My customer is implementing our DDC2256A and would need to get more details on the chip behavior for negative ambient temperatures, for -10°C, -20°C and -30°C:
- does the chip can withstand this temperature…
Part Number: DDC2256A Hi TI‘s expert, I am using DDC2256A along with Altera Cyclone IV GX FPGA. I had several question when I read the datasheet of ddc2256a.
First ,The datasheet shows the min VIH is 0.8DVDD and the max VIL is 0.2DVDD. That is…
Other Parts Discussed in Thread: DDC264 , DDC264EVM , DDC232 , DDC114 , DDC118 , DDC2256A , DDC112 , DDC1128
1. Is the hardware trigger active in the DDC264 evaluation board?
What is the amplitude and shape of the input trigger signal that can be issued into…
Dear Dooho,
the AFE0064, AFE1256, AFE2256 etc. family devices are focused on charge integration. Their target application is charge packets or discrete currents, for example - x-ray panel readout.
Under some special cases, these devices can also be used…
Other Parts Discussed in Thread: DDC2256A , DDC316 , ADC3221 , ADS8168 Hi TI
Is there any digital DDC thip or ADC chip with Integrated DDC for 200K-400Khz using now?
Part Number: DDC2256AEVM Other Parts Discussed in Thread: DDC2256A , Tool/software: Linux
Hi,
Could you send me the reference design with DDC2256A EVM based on Intel Altera FPGA Cyclone 4 FPGA with GUI on PC?
Thanks and best regards,
Bugra
Hi Edu,
Thanks for the info. Excuse the inference, but from the tone of your response it sounds like the DDC is dated component (I know the datasheet is lacking). Would you recommend my using a different part? I am getting pushback on gaining info on…
Other Parts Discussed in Thread: DDC2256A , AFE2256 , AFE0064 , DDC264 Hi Ti
Does TI have sensor solution as below
Sensor circuit design, - For optical sensing array, perform voltage or current sensing, and digitize and store the image as a picture file
Hi Anton,
I would like to take this discussion offline since the device DDC2256A is under NDA.
Please send an email to praveen.aroul@ti.com and mendez@ti.com