Hi Louis,
It looks like one of the redistributables is not installing correctly on your machine. Can you please:
Save the attached file as .exe
Double click on it to run it.
Follow the prompts and report any errors.
If no errors, please delete…
Hi Board designers,
Good to hear on your plan to reuse the SK-AM62B schematics to design the custom board.
Refer below note:
Always refer to the latest design files, for TMDS62LEVM AM62L evaluation module
Refer below recommendations or guidelines…
Hi Tony,
Tony B44 said: can I trade off the bitrate for quality Yes you can control the bitrate & Quality.
You can generate the sample video clips at your platform using the library in .
The user guide in Docs will provide you more details on bitrate…
Part Number: TDA4VM I find yolov3-tiny config file in the path ti_dl/test/testvecs/config/import/public/onnx/tidl_import_tiny_yolo3.txt. If I want use yolov3-tiny model in TDA4, is the darknet version supported?
Now what I have done is that I convert…
Hi Karl,
You're running Windows 7, what's the service pack? We require service pack 1 or higher.
Please post the logfile created (<installdir>/install_logs/MSVC_REDIST_2008.log) here.
I'd like you to run the executable on the command line in interactive…
Part Number: TDA2 Tool/software: TI-RTOS Hello, I'm running the TIDL object detection usecase, and usecase is running fine only with a small problem here:
My original input file is .MP4 with resolution 1920*1080, and I make it to .h264 with resolution…
Hi Mario,
You'll need to install the python module missing via pip (a python package manager) to get rid of the error (crcmod mod in this case).
Perhaps, instead of running the python script through python, use the executable (that already has all…
Could you please try the following:
1. Download the file attached. Change the extension from .txt to .bin
2. Run it from the command line with the following parameters:
"ti_simpack_vayu_ccs_0.6.2.0_setup.bin" --mode silent --prefix "/home/vasanthaangappan…