Christian,
Here are the programming values for the 4 devices. I found an RXDET[0] bit which did not need to be set.
Device 0 ( EQ = 01, VOD = 05, DEM = 02)
00, 00, 04, 07, 00, 01, AD, 40, 00, 1A, D4, 00, 01, AD,
40, 00, 1A, D4, 01, 80, 03, 5A, 80, 00…
Shrikant,
You are correct, the pinout for the SLOU055 board is meant for a pin-out similar to the OPA2836. The evaluation module for the OPA2889 requires the use of the DEM-OPA-MSOP-2B EVM. If you can work with 5V supplies then the OPA2836 can be used…
Hi Brian,
The LM34927 is rated for 600mA of DC output current. The inductor is generally chosen to provide a peak-to-peak ripple current of 30-50% of the rated full-load current. With the minimum current limit setting of 700mA (corresponding to peak…
You can order the EVM from the link below. Click on the "Buy from TI" button:
http://www.ti.com/tool/dem-opa-so-2a?keyMatch=dem-opa-msop-2a&tisearch=Search-EN-Everything
Thanks,
Samir
Other Parts Discussed in Thread: DEM-OPA-SO-1A , OPA656 Hi,
I need a transimpedance amplifier to connect output voltage of AC resistors (value from 10 mohm to 1000 ohm) to PXI 4461 that has 1 MΩ || 217 pF on the inputs. The frequency of interest is 50-100…
Part Number: LM3410 Hello,
I would like to drive 4 Osram SFH 4716AS High power IR LED's /cfs-file/__key/communityserver-discussions-components-files/196/8688.IR_5F00_LED.pdf
My goal is to power these from a 5volt supply, I need to flash them at 1A…
Hello Rakesh,
Unfortunately, we currently don't have an evaluation module/PCB that can accommodate the amplifier AND photodiode. We however have a generic PCB for the OPA659 in a SOT-23 (DBV) package. Please see attached. I would recommend going with…
A decent technician with a hot air gun should be able to solder either the SON or WCSP package.
But if you need an old-school leaded package, we have TPS62160 in an MSOP which does 1A. If you really need a little more than 1A, we have TLV62565/6.
Other Parts Discussed in Thread: DEM-OPA-SO-1A Hello TI engineers
I saw PCB for high speed amplifier DEM-OPA-SO-1A like a picture and I have 2 questions about this design.
1. Why top side has no ground plane?
2. Why ground plane at bottom side blank area…