Aaron,
If a part oscillates, it doesn't necessarily mean that you have damaged the part, however when op-amps oscillate they tend to self-heat and may end up damaging themselves.
Now that you've fixed the gain issue, here's a few other things you…
Application is running off of a 6V supply and generating 5V for a daughter board. Contents of the daughter board can vary.
Vin = 6V
Vout = 5V
Ipeak = ??? (not sure of all possible daughterboard configurations and applications as this point…let…
Victor,
Thank you for your response, I have purchased a few LM3410s (the 8 pin MSOP package) to test. Looking over the datasheet, I wanted to make sure I was understanding things correctly. Pins 3 and 2 should be my Power and Gnd connections respectively…
Part Number: BQ76952 Dear TI engineer,
Like the title, is it supported to use BQ76952's LDO as a driver for RS485 communication current? Will BQ76952 have severe fever?
Attached as RS485 IC specification
Thanks!
Attached as RS485 IC specification…
Part Number: BQ24171 Other Parts Discussed in Thread: BQ29209 Tool/software: Hi, TI E2E
I want to design a Li-Ion battery, but I'm uncertain if the design need to do any more modify?
The design need to do the IEC-62133 verification.
The design…
I started from the PMP7899 project, and I attempted to use the same components..
As you can see in the attached schematic, the most difference between my schematic and the PMP7899 is ISO1, that has same features of isolator used in PMP7899..
AiLux_PoE_PSE…
Part Number: DS100MB203
Tool/software:
Goodday
I have a design that uses the DS100MB203SQ/NOPB as a DEMUX/MUX for 10GBASE-R traffic.
0714.UMAR-10G02.pdf
In summary (see the schematic page attached) the left side goes the host FPGA (S_IN/Out…
Hi Michael,
Yes, those were our default first cut at the SMB settings. Here is a more recent set of settings with the override bits set: The DEMA/B are pulled to 1 by the SDA and SCL pull-up resistors. We are able to pull them down to a more reasonable…
Hello Samir and Livingstone,
In addition to Samir's comments, here are my inputs to your questions:
1) Photodiode / Mimicking a current generator: If you can use an actual photodiode for bench testing, I found some which are close to the 70pF terminal…
Part Number: LM5022 Other Parts Discussed in Thread: TPS40210 , LM5155 Hello TI experts,
my customer wants to find a flyback converter(or controller) for capacitor charging.
they checked the device below several years ago, but they want to use latest…