Part Number: DIR9001 Can DIR9001 ic will support or receive the IEC61937 format and convert into stereo ( I2S )?
since the input is from TV(SPDIF) support Dolby format, whether DIR9001 will receive the signal(SPDIF) and convert to stereo(I2S)?
Part Number: DIR9001 Can DIR9001-Q1 be used to replace DIR9001 in non-automotive applications? The DIR9001 is out of stock while there seems to be a healthy supply of the DIR9001-Q1. The Q1 part is "automotive qualified"
while the data sheet…
Part Number: DIR9001 Hi Team,
my customer is asking if there is a margin about the rise time and fall time of 10ns as shown in the DIR9001 data sheet below:
Their clock source does not meet the spec so far:
They need to adjust their source and they…
Part Number: DIR9001 Other Parts Discussed in Thread: DIT4096 Hi team,
My customer have the DIR9001 to receive a SPDIF signal and transmit that data to the DIT4096 via I2S. Then the DIT4096 outputs the SPDIF signal to some external receiver.
What is t…
Part Number: DIR9001 Other Parts Discussed in Thread: SRC4382 , SRC4192 , SRC4190 Hi Experts,
Good day and allow me to post this case from client.
Customer is in the development process of a beamforming speaker for professional audio applications. Asking…
Part Number: DIR9001 Hi Team,
DIR9001 has an S/PDIF input port, which can be directly input when it is an Optical S/PDIF inputs signal.
Why do you need to add a buffer amplifier might be required between the optical receiver module output and the DIR9001…
Part Number: DIR9001 Hi Sir,
Pls kindly help for below questions for DIR9001, thanks.
What different between PLL "lock" and "unlock"? How to switch between?
AUDIO and EMPH are channel status, what function for these two pins?
COUT…
Part Number: DIR9001 Other Parts Discussed in Thread: PCM1794 , PCM1794A Hi, First I'm a little confused by the documentation with regards to crystal or PPL selection. One diagram on the web has a crystal used and the CLKSEL pin floating (so ground by pulldown…
Part Number: DIR9001 Hello,
I am trying to use the DIR9001 in PLL-only-mode, according to the schematics below.
When I apply an optical signal to my TOSLINK receiver, the PLL locks, and I get valid outputs on FSOUT0/FSOUT1, depending on the input format…
Part Number: DIR9001 Other Parts Discussed in Thread: PCM1794A , DIX4192 , DIX9211 I finished my project with DIR9001 and PCM1794A and to my surprise, DIR9001 worked just fine with 24bit/192KHz audio signals from SPDIF, although it's rated as 96KHz in the…