Part Number: DIT4096
Hi team, customer uses DIT4096 on the new application. However, customer has the Tx overshoot issues. Here is the waveform. the over shoot voltage is over 6V.
Please refer to the schematic and provide your comments. txn.box.com/.../…
Part Number: DIT4096
Hi Team, Customer uses DIT4096 and found the output is only mono output. The I2S in only provide to DIT4096, there are other I2S DAC in the system. other I2S slave can output stereo nomal. Could you please review the schematic for this…
Part Number: DIT4096 Hi team,
I'm interested in using DIT4096 in an application where the I2S source will be a Bluetooth module. The BT module format may change, but the base mode is as follows:
BT module = master, DIT4096 = slave
16-bit I2S
BCK…
Part Number: DIT4096
Hi Team, Cusotmer uses DIT4096 for the SW mode setting. The audio source is stereo 1. I2S 16bit setting. 2. WCLK is 48KHz. 3. MCLK is 128fs
Questions: 1. Can HW mode support this audio source format? 2. if HW cannot support, how to set…
Part Number: DIT4096 Other Parts Discussed in Thread: PCM4201 , PCM4201EVM
Hi Team, Customer uses DIT4096 and has some issues. Thus, we used the PCM4201 EVM's DIT4096 for verification.
schematic www.ti.com/.../sbau108
I jumped the RN4 and RN3 resistor…
Part Number: DIT4096
Hi Team,
When working with the DIT4096 configured in I2S slave mode and driven from a Bluetooth module with I2S audio outputs, do the I2S input signals need to be synchronous to its local master lock input? The DIT4096 local master…
Part Number: DIT4096
Hi Team, Nvidea chip out the following I2S format. 1. I2S digital out. 2. 16b/sample 3. MSB first
Here is the DIT4096 format selection. Could you please let me know which mode can support the the Nvidia output format?
Thanks, SHH
Part Number: DIT4096
Hi Team,
customer would like to use DIT4096. could you please help review the DIT4096 schematic?
password: "ti"
5265.DIT4096.7z
here is the light transmitter. please provide your comment if this is not ok.
6518.2B.13157…
Part Number: DIT4096 Hi TI audio expert,
One of my customer is designing the DIT4096 in their system, they used the software mode. I have searched in TI website, I didn't found anything talking about the configuration of DIT4096 in software mode. So…
Part Number: DIT4096 I want to use DIT4096 in slave mode to interface with a Bluetooth SOC which is a master from I2S interface perspective. The design is to support 48KHz sampling rate and 16-bit audio data. DIT4096 will convert the I2S digital audio…