Part Number: DIT4096 Why Sampling Frequency is changed from 44.1kHz to 48kHz?
I'm Japanese. I'm sorry my poor English.
I have evaluated DIT4096.
<My Constitution>
I2S(44.1kHz) → DIT4096 → SPDIF(48kHz)
<My Demand> ・Consumer mode ・Sampling…
Part Number: DIT4096 Other Parts Discussed in Thread: DIT4192 Hi Team,
Can DIT4096 support I2S to SPDIF converter? SPDIF is 5.1 output of product spec.
Thanks,
SHH
Other Parts Discussed in Thread: DIT4096 , SRC4190 Hi,
I am designing a device which can transfers USB audio to AES-3 output by connecting PCM2707 and DIR4096 in their I2S features.
Since I want to limit the hardware components numbers, I selected hardware…
Hi Colin,
Sorry to hear that. Please feel free to come back with any additional questions you have, if you have time to take another look there is an EVM Users Guide you can compare your setup/PCB schematic to: www.ti.com/.../sbau108a.pdf
Justin
Other Parts Discussed in Thread: DIT4192 , DIT4096 , DIX4192 Hey team,
I want to use DIT4096 or DIT4192 as I2S input, S/PDIF output converter. Can I do that? It seems that since they are listed as having AES3 capable outputs that it would be possible but…
Other Parts Discussed in Thread: DIT4096 , DRV134 , SN75176B Hi,
Do you have any products with same function only like the internal line driver of DIT4096? Could you please tell me if you have?
Best Regards, Kato
Other Parts Discussed in Thread: DIT4096 I am planning to use a DIT4096 in HW mode and would like to use the reset line to disable the output. i.e. If I don't want to send a s/pdif signal out I will just pull the reset line low indefinitely . I just…
Other Parts Discussed in Thread: DIT4096 Hi,
The datasheet of DIT4096 has no recommended operating condition, but I understand that the recommended supply voltage is Vdd=5.0V. So it can not be operated from Vdd=3.3V. Is my understanding correct?
Then is…
Other Parts Discussed in Thread: DIR9001 , DIT4096 I have an issue where the data from a DIT4096 on one card is being received by a DIR9001 on another and the Error flag is oscillating in sympathy with the blocks of data;
clutching at straws before taking…
Other Parts Discussed in Thread: DIT4192 , DIT4096 All the reference designs from TI based on DIT4096 and DIT4192 use TX+ pin for SPDIF Optical out and TX- for SPDIF Coaxial out when both optical and coaxial outputs are provided. Is there any significance…