Other Parts Discussed in Thread: DRV8312 hello, I recently received my DK-LM4F211-DRV8312 Motor Control Development Kit and am very enthusiastic about the possibilities! Now I have a BLDC motor with 36 input votage and I want to power this motor via DK…
Hi
The application AN01289 shows how to compile a project InstaSpin_BuildLevels
for CCS4.
Is it possible to compile the code to work for Keil ?.
Will the librray will work ?.
Please Advise.
Ephraim Oved.
Hi Martin,
I have done it yesterday, just like you said. So firstly tried the update, but promlem was not solved. After that downloaded v5.3, now it runs convenient. Thank you for your response.
Mete
Other Parts Discussed in Thread: DRV8412 , DRV8312 Page 3 of The Baseboard Hardware Reference Guide for the DK-LM3S-DRV8312 brushed motor kit mentions that it is possible to connect 2 brushed DC motors to the kit’s board and refers to Figure 5.
There…
Tony,
You should find everything you need at the link below. Click the "Get Software" button. Reply to the questionaire and it will download everything you need.
http://www.ti.com/tool/dk-lm4f-drv8312-cd
Other Parts Discussed in Thread: INSTASPIN-BLDC TI,
I am attempting to rebuild the libbuild project on with the software CD supplied with DK-LM4F-DRV8312.
The project cannot find "InstaSPIN_BLDC.c":
The source does not appear to be on the supplied…
Milan,
Thank you for your answer.
Which evaluation board do you suggest me, DK-LM4F-DRV8312 or DRV8301-HC-C2-KIT ?
With DK-LM4F-DRV8312 :
1) I will be able to test LM4F and DRV8312. But I don't know If my conclusions with DRV8312, should be the…
Hi Matt,
Indeed, I have the C2000 DRV8312-69M-KIT (Motor: DT4260-24-055-04H-PT) , I have an USB and a CD, in the USB I can't find the motor specs and unfortunately I can't read Cd's in my laptop... I'm using the specs of the Motor DT4260-24-055-04H…
Other Parts Discussed in Thread: DRV8312 Hi!
I have started designing a controller for Hall Sensor commuted small BLDC motor. In order to evaluate the software and parameters, as well as HW (such as DRV83x2), I have ordered a DK-LM4F-DRV8312 - 3-Phase…
Other Parts Discussed in Thread: DRV8312 HI,
A small query customer already purchased DK-LM4F-DRV8312
Now he wants with sensor BLDC solution for that he requested for suggesting the plug-in board from C2000 with on board emulator to use on the same…