Part Number: DK-TM4C123G Does anyone know why TI disgnated the DK-TM4C123G obsolete? I think it is a great development kit. One of the best for CAN development. Is there a newer kit in the TM4C123G series for CAN development?
Thanks,
Dave
Part Number: DK-TM4C123G I'm on Windows 10 with UniFlash v4 trying to load an image (or even just verify an image) but get the error message "Cannot read property 'DS' of undefined". I'm not really sure how to troubleshoot this. I know that UniFlash v4…
Part Number: DK-TM4C123G Dear team:
Do you have another development kit for CAN protocol similar to the following?: TM4C123G USB CAN Development Kit DK-TM4C123G
Best regards
Part Number: EK-TM4C123GXL
I have recently bought a BOOSTXL-SENSHUB and had interest in using its MPU-9150 with my EK-TM4C123GXL. The example available in CCS that makes use of the MPU-9150 works as intended, but it's a non-rtos example. I am planning…
Good morning Ralph,
I have provided the images requested with the debug output for IAR provided instead of the debug output for CCS. I provided the picture with IAR as that is the environment that I am required to use. If preferable, I can recapture…
Hi,
Maheedh Mohamed1 said: I have seen a sample project(data-logger) for DK-TM4C123GXL but that code is not compatible with EK-tm4c123gxl.
Do you mean DK-TM4C1294XL or DK-TM4C123G? There is no DK-TM4C123GXL but only EK-TM4C123GXL. If you mean DK-TM4C123G…
Part Number: DK-TM4C123G Hi,
I am trying to set up CAN demo on two DK-TM4C123G demo boards. I have added two 120ohm resistors to both sides. The data did send from TX side and I can measure it on CAN wire. I also measure the signal between CAN transceiver…
Part Number: SW-DK-TM4C123G Hi:
I am writing a very simple piece of code to enable the GPIO on pin 4 of Port M. The code is below. To make sure, I created a new program that ONLY has the code below. The issue I am having is that the GPIOPinTypeGPIOInput…