Part Number: DLP3021LEQ1EVM Hey,
DLP Composer does not seem to have any projects.
How do I open the DGP LED Project? In order to access the EVM resources and be able to change settings?
Other Parts Discussed in Thread: DLP3010EVM-LC The DLP DLCR 3010 EVM - G2 has output 300 lumens.
DLP 3010 EVM LC mentions 125 lumens.
Meaning the brightness value 299 lumens mentioned in PDF DLPA079 is for DLP DLCR 3010 EVM - G2 or DLP 3010 EVM LC?
Dear Aron,
First of all, I sincerely thank you for deciding to provide technical support.
As you mentioned, 15W is indeed a relatively low power source. However, we made the request considering that the resolution of the DLP we are using is low, and the…
Hello Junfa,
As your test states, you don't turn off the DMD, so I don't see this as a power down issue at all.
junfa ye said: The aging process is to switch to the dark field observation picture with low LED current. After no defects are found…
Hello User,
Welcome back to the E2E forums and thank you for your interest in TI DLP ® Technology.
It sounds like you may want a light control specific EVM and for the lumens requirement of 100 lumens, the DLP3010EVM-LC may be your best choice still…
Thank you for your reply.
I would like to describe our task more detailly.
I want to customize the DGP device based on the DLP2021.
My DGP device can be flashed via CAN communication (destop_r32.bin, image, video etc.).
Currently, the DLP composer using…
Hello User,
Welcome to the E2E forums and thank you for your interest in DLP ® technology.
I just want to double check that this is a custom system you have designed and not the DLPDLCR2010EVM? If it is a custom design were you basing it off of this…
Hi Xiaoqiang,
Thanks for sending the files! I don't see anything in your build log indicating a failure; can you verify whether or not you have a binary file located in <project dir>/Outputs? It should be called FlashImage.img.
I've also imported…
Part Number: DLP670RE Other Parts Discussed in Thread: DLP801RE , DLP800RE , DLPC4420AEVM , DLP780TE , DLPC7540EVM , DLP650TE , DLP650TEEVM , DLPC7540 Tool/software: Hi,TI Team:
I want to select high brightness DLP product for our projector , I find display…