Part Number: DLPC4422 Other Parts Discussed in Thread: DLP660TE , Hi TI
hardware platform:4K UHD High Brightness Display Reference Design using TI DLP® Technology
http://www.ti.com/product/DLPC4422/toolssoftware
Firmware version :DLP660TE_Chipset_Firmware_v8…
Hi Jason, first of all thank you very much for your reply, in order to modify a DLP5531LEQ1EVM to suit our needs (use external video and have a set brightness on startup) we were given acces to the DLP composer tool and some proyects that could be used…
Part Number: DLP3010 Tool/software: Hello, Ti team.
Our company produces DLP optical machines and has considerable industry experience.
As we all know, DMD is easy to be damaged and produce bad points.
There are many reasons for production, such as static…
Hi Oben,
Here is an example where TPS92641 is used to output max 20A current - DLP® Pico Brightness Turbo and TPS92641 Design Guide (ti.com) .
Best Regards,
Steven
Part Number: DLP5531LEQ1EVM Hello, in order to modify a DLP5531LEQ1EVM to suit our needs (use external video and have a set brightness on startup) we were given acces to the DLP composer tool and some proyects that could be used to modify its behaviour…
Part Number: DLPC4430 Other Parts Discussed in Thread: DLP650LE Tool/software: Hello, TI.
I would like to talk for reducing spoke size. I have faced two issues trying to redulce the spoke size from 12.0 to 4.00 degree.
The configuration I'm using are…
Part Number: DLP3021-Q1 Other Parts Discussed in Thread: DLP3021LEQ1EVM , DLPC120-Q1
[PAGE UNDER CONSTRUCTION]
This FAQ page is intended to serve as a complete guide for users evaluating and developing Dynamic Ground Projection (DGP) solutions. The DLP3021…
Hello User,
Welcome to the E2E forum.
We do not allow for LED current adjustments continuously from 0 to 100%. There is a feedback loop wherein the DLP circuitry monitors the current being driven via the illuminators. If the driven current is too low…
Hello Zhangyuzhen,
A couple of quick questions:
By "blank" pattern do you mean an all "off" pattern? I assume so since the mirrors will be tilted away from the beam at 12 degrees so that the reflected angle will be at - the incident…
Part Number: DLP4710EVM-LC Hello,
We are using a DLP in a unique application where we need to maintain high frequency content on our output projected light. Ideally we would need >2 kHz frequency content.
After reading some papers on DMDs I see there…