Hi Yang,
Issue 1:
This issue may be hard to debug as the signals to check the external parallel hdmi are vsync, hsync, and Pclk but are not easily accessible on the EVM. Do you have access to an oscilloscope? We know that the RMA process is complicated…
Hello,
The AR HUD Lumen Budget Estimation Calculator can be found at the link below.
http://www.ti.com/tool/DLP-HUD-LUMEN-CALC
There are two automotive qualified DMDs for AR-HUD applications. The DLP3030-Q1 offers an output resolution of 864x480. The…
Part Number: DLP3030CHUDQ1EVM We are looking for combiner HUD similar to DLP3030CHUDQ1EVM with following specification
HUD – with 1 or 3 glass pieces of 8mm thickness, size of glass : 210mm x 245mm
Input – DVI/HDMI
Resolution – 1280x1024…
Hello Samson,
The LS_SENSE feature is specific to a HUD application, which is why the DLP5531Q1 HL Driver EVM does not utilize these signals, but it can still be optionally monitored in a headlight application. Our default simplified recommendation per…
I am new process development engineer responsible for adhesive processing. We produce loudspeakers for the automotive industry. We are interested to learn about the TI DLP technology. Our Application would firstly be to calculate the volume of a dispensed…
Check the component losses vs. load current with the quickstart calculator. Also, use the inductor vendor's loss estimator for that specific inductor. The inductor looks very large with lower DCR than necessary (high core volume increases core losses…
Hello Sam,
Thank you for your patience.
The product concept looks exciting and the requirements for an optical engine are challenging.
I am not aware of an existing optical engine which can meet your requirement. You need to work a design house or an…
A.
Thank you for the clarification. I believe I understand. between the DMD/prism assembly, and the series of mirrors that direct the image onto the HUD you wonder if a single lens is acceptable as a means to enlarge the image.
I again reached out to our…
Hello Vladimir,
It is not common that we give out composer licenses to customers unless you can show intent to use significant volume of DLP chips. And most firmware changes desired by customers are simple and we can create them for you in a short time…
Part Number: DLP3021-Q1 Other Parts Discussed in Thread: DLPC120-Q1
[PAGE UNDER CONSTRUCTION]
This FAQ page is intended to serve as a complete guide for users evaluating and developing Dynamic Ground Projection (DGP) solutions. The DLP3021-Q1 is the…