Part Number: DLPC3479 Other Parts Discussed in Thread: DLPA3005 , Dear all,
We are developing pico-projectors based on the DLP3479 chips, and looking for an older version firmware as we used to.
At TI DLP® Pico Firmware Selector https://software-dl.ti…
Hi Jimmy,
To confirm, you have an original DLP3010EVM (not G2 version)? If so, this product is End-of-Life and has been superseded by the DLP3010EVM-G2. For such reason and numerous changes made between both systems, the original firmware is no longer…
Hello,
I see you are currently using fw version 8.1.0. I would first suggest updating your firmware to the latest version (v8.1.1), which can be found on the TI DLP Pico FW Selector Tool . Additionally could you provide the test patterns you are trying…
Hello Michael,
thank you so much for the thorough explanation! Yes, this definitely helps me and and we can make the decision from here on. I have checked the DLP Pico products and unfortunately they have a smaller than desired number of pixels. I think…
Hi Oben,
Here is an example where TPS92641 is used to output max 20A current - DLP® Pico Brightness Turbo and TPS92641 Design Guide (ti.com) .
Best Regards,
Steven
Part Number: DLPC3478 I've meet some problem while using DLP-PICO-DLPC34XX-API. I can't built it on x64 platform. I noticed that the original cyusbserial.dll & cyusbserial.lib are x86 version. So I try to use x64 version instead. But it still…
Part Number: DLP4710EVM-LC The EVM status shows Connected, Powered off. I had tried to reset the projector power and switch on and off the projector switch. The EVM status still shows the same status issue, it shows Connected, Powered off. What can I…
Dear Rusi
Thank you for your kind support !!
1) Yes. The issue is solved using FWSel_DLPC3478_DLPA2005_pm1_i2c0x36_v9p0p1.img and DLP GUI version 3.2.0.6
2) I have final Questions.
Q1) What is a difference between DLP3010EVM-LC_9.0.1.img and FWSel_DLPC3478_DLPA2005_pm1_i2c0x36_v9p0p1…
DLP-PICO-BOOT-DIAGNOSTIC-TOOL — DLP Pico Boot Diagnostic Tool,I use it, but it tell me fail. I guess this may be the failure because the three voltage signals DMD_VOFFSET, DMD_VBIAS, and DMD_VRESET are not output.